Public Attributes#

uint8_t
uint8_t
union rsi_rsp_dns_query_s::@4

Public Attribute Documentation#

ip_version#

uint8_t ip_version[2]

Definition at line 336 of file include/rsi_nwk.h

ip_count#

uint8_t ip_count[2]

Definition at line 339 of file include/rsi_nwk.h

ipv4_address#

uint8_t ipv4_address[4]

Definition at line 343 of file include/rsi_nwk.h

ipv6_address#

uint8_t ipv6_address[16]

Definition at line 344 of file include/rsi_nwk.h

ip_address#

union rsi_rsp_dns_query_s::@4 ip_address[MAX_DNS_REPLIES]

Definition at line 345 of file include/rsi_nwk.h