Structure representing HTTP server request parameters.

This structure holds the parameters for an HTTP server request, including the request URI, HTTP version, headers, request type, and data length.

Public Attributes#

URI of the request, including path and query parameters.

HTTP protocol version (for example, HTTP/1.1, HTTP/2).

uint16_t

Number of request headers received.

Type of the request (for example, GET, POST, PUT, DELETE).

uint32_t

Length of the request data in bytes.

Public Attribute Documentation#

uri#

sl_http_server_request_uri_t sl_http_server_request_s::uri

URI of the request, including path and query parameters.


version#

sl_http_request_version_t sl_http_server_request_s::version

HTTP protocol version (for example, HTTP/1.1, HTTP/2).


request_header_count#

uint16_t sl_http_server_request_s::request_header_count

Number of request headers received.


type#

sl_http_server_request_type_t sl_http_server_request_s::type

Type of the request (for example, GET, POST, PUT, DELETE).


request_data_length#

uint32_t sl_http_server_request_s::request_data_length

Length of the request data in bytes.