Structure to hold the threshold detection configuration parameters.
Public Attributes#
uint8_t *
Threshold_1 condition like Equal, Grater, Lesser.
uint8_t *
Threshold_2 condition like Equal, Grater, Lesser.
Public Attribute Documentation#
threshold1#
uint16_t sl_adc_threshold_config_t::threshold1
Threshold_1.
threshold2#
uint16_t sl_adc_threshold_config_t::threshold2
Threshold_2.
threshold1_cond#
uint8_t* sl_adc_threshold_config_t::threshold1_cond
Threshold_1 condition like Equal, Grater, Lesser.
threshold2_cond#
uint8_t* sl_adc_threshold_config_t::threshold2_cond
Threshold_2 condition like Equal, Grater, Lesser.
range#
uint8_t sl_adc_threshold_config_t::range