IOT Sockets#

The IOT socket implementation aims to emulate the standards library to the extent possible for embedded offerings from Silabs. There are substantial limitation/exceptions however, and those are mentioned in the subsequent documentation of IOT sockets.

Functions#

int32_t
iotSocketCreate(int32_t af, int32_t type, int32_t protocol)

Create a communication socket.

int32_t
iotSocketBind(int32_t socket, const uint8_t *ip, uint32_t ip_len, uint16_t port)

Assign a local address to a socket.

int32_t
iotSocketListen(int32_t socket, int32_t backlog)

Listen for socket connections.

int32_t
iotSocketAccept(int32_t socket, uint8_t *ip, uint32_t *ip_len, uint16_t *port)

Accept a new connection on a socket.

int32_t
iotSocketConnect(int32_t socket, const uint8_t *ip, uint32_t ip_len, uint16_t port)

Connect a socket to a remote host.

int32_t
iotSocketRecv(int32_t socket, void *buf, uint32_t len)

Receives data from the socket.

int32_t
iotSocketRecvFrom(int32_t socket, void *buf, uint32_t len, uint8_t *ip, uint32_t *ip_len, uint16_t *port)

Receives data from the socket.

int32_t
iotSocketSend(int32_t socket, const void *buf, uint32_t len)

Send data or check if data can be sent on a connected socket.

int32_t
iotSocketSendTo(int32_t socket, const void *buf, uint32_t len, const uint8_t *ip, uint32_t ip_len, uint16_t port)

Send data or check if data can be sent on a socket.

int32_t
iotSocketGetSockName(int32_t socket, uint8_t *ip, uint32_t *ip_len, uint16_t *port)

Retrieve local IP address and port of a socket.

int32_t
iotSocketGetPeerName(int32_t socket, uint8_t *ip, uint32_t *ip_len, uint16_t *port)

Retrieve remote IP address and port of a socket.

int32_t
iotSocketGetOpt(int32_t socket, int32_t opt_id, void *opt_val, uint32_t *opt_len)

Get socket option.

int32_t
iotSocketSetOpt(int32_t socket, int32_t opt_id, const void *opt_val, uint32_t opt_len)

Set socket option.

int32_t
iotSocketClose(int32_t socket)

Close and release a socket.

int32_t
iotSocketGetHostByName(const char *name, int32_t af, uint8_t *ip, uint32_t *ip_len)

Retrieve host IP address from host name.

Function Documentation#

iotSocketCreate#

int32_t iotSocketCreate (int32_t af, int32_t type, int32_t protocol)

Create a communication socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]af

address family.

int32_t[in]type

socket type.

int32_t[in]protocol

socket protocol.

Returns

  • status information:

    • Socket identification number (>=0).

    • IOT_SOCKET_EINVAL = Invalid argument.

    • IOT_SOCKET_ENOTSUP = Operation not supported.

    • IOT_SOCKET_ENOMEM = Not enough memory.

    • IOT_SOCKET_ERROR = Unspecified error.


iotSocketBind#

int32_t iotSocketBind (int32_t socket, const uint8_t * ip, uint32_t ip_len, uint16_t port)

Assign a local address to a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

const uint8_t *[in]ip

pointer to local IP address.

uint32_t[in]ip_len

length of 'ip' address in bytes.

uint16_t[in]port

local port number.

Returns

  • status information:

    • 0 = Operation successful.

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument (address or socket already bound).

    • IOT_SOCKET_EADDRINUSE = Address already in use.

    • IOT_SOCKET_ERROR = Unspecified error.


iotSocketListen#

int32_t iotSocketListen (int32_t socket, int32_t backlog)

Listen for socket connections.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

int32_t[in]backlog

maximum number of the clients supported.

Returns

  • status information:

    • 0 = Operation successful.

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument (socket not bound).

    • IOT_SOCKET_ENOTSUP = Operation not supported.

    • IOT_SOCKET_EISCONN = Socket is already connected.

    • IOT_SOCKET_ERROR = Unspecified error.


iotSocketAccept#

int32_t iotSocketAccept (int32_t socket, uint8_t * ip, uint32_t * ip_len, uint16_t * port)

Accept a new connection on a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

uint8_t *[out]ip

pointer to buffer where address of connecting socket shall be returned (NULL for none).

uint32_t *[inout]ip_len

pointer to length of 'ip' (or NULL if 'ip' is NULL):

  • length of supplied 'ip' on input.

  • length of stored 'ip' on output.

uint16_t *[out]port

pointer to buffer where port of connecting socket shall be returned (NULL for none).

Returns

  • status information:

    • socket identification number of accepted socket (>=0).

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument (socket not in listen mode).

    • IOT_SOCKET_ENOTSUP = Operation not supported (socket type does not support accepting connections).

    • IOT_SOCKET_ECONNRESET = Connection reset by the peer.

    • IOT_SOCKET_ECONNABORTED = Connection aborted locally.

    • IOT_SOCKET_EAGAIN = Operation would block or timed out (may be called again).

    • IOT_SOCKET_ERROR = Unspecified error.


iotSocketConnect#

int32_t iotSocketConnect (int32_t socket, const uint8_t * ip, uint32_t ip_len, uint16_t port)

Connect a socket to a remote host.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

const uint8_t *[in]ip

pointer to remote IP address.

uint32_t[in]ip_len

length of 'ip' address in bytes.

uint16_t[in]port

remote port number.

Returns

  • status information:

    • 0 = Operation successful.

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument.

    • IOT_SOCKET_EALREADY = Connection already in progress.

    • IOT_SOCKET_EINPROGRESS = Operation in progress.

    • IOT_SOCKET_EISCONN = Socket is connected.

    • IOT_SOCKET_ECONNREFUSED = Connection rejected by the peer.

    • IOT_SOCKET_ECONNABORTED = Connection aborted locally.

    • IOT_SOCKET_EADDRINUSE = Address already in use.

    • IOT_SOCKET_ETIMEDOUT = Operation timed out.

    • IOT_SOCKET_ERROR = Unspecified error.


iotSocketRecv#

int32_t iotSocketRecv (int32_t socket, void * buf, uint32_t len)

Receives data from the socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

void *[out]buf

pointer to buffer where data should be stored.

uint32_t[in]len

length of buffer (in bytes).

Returns

  • status information:

    • number of bytes received (>=0), if len != 0.

    • 0 = Data is available (len = 0).

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument (pointer to buffer or length).

    • IOT_SOCKET_ENOTCONN = Socket is not connected.

    • IOT_SOCKET_ECONNRESET = Connection reset by the peer.

    • IOT_SOCKET_ECONNABORTED = Connection aborted locally.

    • IOT_SOCKET_EAGAIN = Operation would block or timed out (may be called again).

    • IOT_SOCKET_ERROR = Unspecified error.


iotSocketRecvFrom#

int32_t iotSocketRecvFrom (int32_t socket, void * buf, uint32_t len, uint8_t * ip, uint32_t * ip_len, uint16_t * port)

Receives data from the socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

void *[out]buf

pointer to buffer where data should be stored.

uint32_t[in]len

length of buffer (in bytes).

uint8_t *[out]ip

pointer to buffer where remote source address shall be returned (NULL for none).

uint32_t *[inout]ip_len

pointer to length of 'ip' (or NULL if 'ip' is NULL):

  • length of supplied 'ip' on input.

  • length of stored 'ip' on output.

uint16_t *[out]port

pointer to buffer where remote source port shall be returned (NULL for none).

Returns

  • status information:

    • number of bytes received (>=0), if len != 0.

    • 0 = Data is available (len = 0).

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument (pointer to buffer or length).

    • IOT_SOCKET_ENOTCONN = Socket is not connected.

    • IOT_SOCKET_ECONNRESET = Connection reset by the peer.

    • IOT_SOCKET_ECONNABORTED = Connection aborted locally.

    • IOT_SOCKET_EAGAIN = Operation would block or timed out (may be called again).

    • IOT_SOCKET_ERROR = Unspecified error.


iotSocketSend#

int32_t iotSocketSend (int32_t socket, const void * buf, uint32_t len)

Send data or check if data can be sent on a connected socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

const void *[in]buf

pointer to buffer containing data to send.

uint32_t[in]len

length of data (in bytes).

Returns

  • status information:

    • number of bytes sent (>=0), if len != 0.

    • 0 = Data can be sent (len = 0).

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument (pointer to buffer or length).

    • IOT_SOCKET_ENOTCONN = Socket is not connected.

    • IOT_SOCKET_ECONNRESET = Connection reset by the peer.

    • IOT_SOCKET_ECONNABORTED = Connection aborted locally.

    • IOT_SOCKET_EAGAIN = Operation would block or timed out (may be called again).

    • IOT_SOCKET_ERROR = Unspecified error.

Note

  • The iotSocketSend() system call doesn't guarantees the packets are transmitted to remote note, which are enqueued in the queue. The iotSocketSend() system call can only send max of 1460 bytes incase of plain TCP, UDP. Whereas incase of TLS, the max buffer length is 1370.


iotSocketSendTo#

int32_t iotSocketSendTo (int32_t socket, const void * buf, uint32_t len, const uint8_t * ip, uint32_t ip_len, uint16_t port)

Send data or check if data can be sent on a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

const void *[in]buf

pointer to buffer containing data to send.

uint32_t[in]len

length of data (in bytes).

const uint8_t *[in]ip

pointer to remote destination IP address.

uint32_t[in]ip_len

length of 'ip' address in bytes.

uint16_t[in]port

remote destination port number.

Note

  • If number of bytes to be send exceeds the MSS size specified by remote node then API will return IOT_SOCKET_ERROR. To know the MSS size for the socket use si91x_get_socket_mss() utility, In case of TCP this should be called after the connect()

Returns

  • status information:

    • number of bytes sent (>=0), if len != 0.

    • 0 = Data can be sent (len = 0).

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument (pointer to buffer or length).

    • IOT_SOCKET_ENOTCONN = Socket is not connected.

    • IOT_SOCKET_ECONNRESET = Connection reset by the peer.

    • IOT_SOCKET_ECONNABORTED = Connection aborted locally.

    • IOT_SOCKET_EAGAIN = Operation would block or timed out (may be called again).

    • IOT_SOCKET_ERROR = Unspecified error.

Note

  • The iotSocketSendTo() system call doesn't guarantees the packets are transmitted to remote note, which are enqueued in the queue. The iotSocketSendTo() system call can only send max of 1460 bytes incase of plain TCP, UDP. Whereas incase of TLS, the max buffer length is 1370.


iotSocketGetSockName#

int32_t iotSocketGetSockName (int32_t socket, uint8_t * ip, uint32_t * ip_len, uint16_t * port)

Retrieve local IP address and port of a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

uint8_t *[out]ip

pointer to buffer where local address shall be returned (NULL for none).

uint32_t *[inout]ip_len

pointer to length of 'ip' (or NULL if 'ip' is NULL):

  • length of supplied 'ip' on input.

  • length of stored 'ip' on output.

uint16_t *[out]port

pointer to buffer where local port shall be returned (NULL for none).

Returns

  • status information:

    • 0 = Operation successful.

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument (pointer to buffer or length).

    • IOT_SOCKET_ERROR = Unspecified error.


iotSocketGetPeerName#

int32_t iotSocketGetPeerName (int32_t socket, uint8_t * ip, uint32_t * ip_len, uint16_t * port)

Retrieve remote IP address and port of a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

uint8_t *[out]ip

pointer to buffer where remote address shall be returned (NULL for none).

uint32_t *[inout]ip_len

pointer to length of 'ip' (or NULL if 'ip' is NULL):

  • length of supplied 'ip' on input.

  • length of stored 'ip' on output.

uint16_t *[out]port

pointer to buffer where remote port shall be returned (NULL for none).

Returns

  • status information:

    • 0 = Operation successful.

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument (pointer to buffer or length).

    • IOT_SOCKET_ENOTCONN = Socket is not connected.

    • IOT_SOCKET_ERROR = Unspecified error.


iotSocketGetOpt#

int32_t iotSocketGetOpt (int32_t socket, int32_t opt_id, void * opt_val, uint32_t * opt_len)

Get socket option.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

int32_t[in]opt_id

option identifier.

void *[out]opt_val

pointer to the buffer that will receive the option value.

uint32_t *[inout]opt_len

pointer to length of the option value:

  • length of buffer on input.

  • length of data on output.

Returns

  • status information:

    • 0 = Operation successful.

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument.

    • IOT_SOCKET_ENOTSUP = Operation not supported.

    • IOT_SOCKET_ERROR = Unspecified error.

Note

  • The following are the options, which are supported currently.

    • IOT_SOCKET_IO_FIONBIO

    • IOT_SOCKET_SO_RCVTIMEO

    • IOT_SOCKET_SO_SNDTIMEO

    • IOT_SOCKET_SO_KEEPALIVE

    • IOT_SOCKET_SO_TYPE.


iotSocketSetOpt#

int32_t iotSocketSetOpt (int32_t socket, int32_t opt_id, const void * opt_val, uint32_t opt_len)

Set socket option.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

int32_t[in]opt_id

option identifier.

const void *[in]opt_val

pointer to the option value.

uint32_t[in]opt_len

length of the option value in bytes.

Returns

  • status information:

    • 0 = Operation successful.

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EINVAL = Invalid argument.

    • IOT_SOCKET_ENOTSUP = Operation not supported.

    • IOT_SOCKET_ERROR = Unspecified error.

Note

  • The following are the options, which are supported currently.

    • IOT_SOCKET_IO_FIONBIO

    • IOT_SOCKET_SO_RCVTIMEO

    • IOT_SOCKET_SO_SNDTIMEO

    • IOT_SOCKET_SO_KEEPALIVE

    • IOT_SOCKET_SO_TYPE.


iotSocketClose#

int32_t iotSocketClose (int32_t socket)

Close and release a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]socket

socket identification number.

Returns

  • status information:

    • 0 = Operation successful.

    • IOT_SOCKET_ESOCK = Invalid socket.

    • IOT_SOCKET_EAGAIN = Operation would block (may be called again).

    • IOT_SOCKET_ERROR = Unspecified error.

Note

  • Calling close on server or first client socket would end up closing othet socket as well.


iotSocketGetHostByName#

int32_t iotSocketGetHostByName (const char * name, int32_t af, uint8_t * ip, uint32_t * ip_len)

Retrieve host IP address from host name.

Parameters
TypeDirectionArgument NameDescription
const char *[in]name

host name.

int32_t[in]af

address family.

uint8_t *[out]ip

pointer to buffer where resolved IP address shall be returned.

uint32_t *[inout]ip_len

pointer to length of 'ip':

  • length of supplied 'ip' on input.

  • length of stored 'ip' on output.

Returns

  • status information:

    • 0 = Operation successful.

    • IOT_SOCKET_EINVAL = Invalid argument.

    • IOT_SOCKET_ENOTSUP = Operation not supported.

    • IOT_SOCKET_ETIMEDOUT = Operation timed out.

    • IOT_SOCKET_EHOSTNOTFOUND = Host not found.

    • IOT_SOCKET_ERROR = Unspecified error.