Definitions for stack tokens. See Stack Tokens for documentation.
The file token-stack.h should not be included directly. It is accessed by the other token files.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef DEFINEADDRESSES
#define TOKEN_NEXT_ADDRESS(region, address)
#endif
// The basic TOKEN_DEF macro should not be used directly since the simplified
// definitions are safer to use. For completeness of information, the basic
// macro has the following format:
//
// TOKEN_DEF(name,creator,iscnt,isidx,type,arraysize,...)
// name - The root name used for the token
// creator - a code used to uniquely identify the token when using SimEE
// nvm3key - a key used to uniquely identify the token when using NVM3
// iscnt - a bool flag that is set to identify a counter token
// isidx - a bool flag that is set to identify an indexed token
// type - the basic type or typdef of the token
// arraysize - the number of elements making up an indexed token
// ... - initializers used when reseting the tokens to default values
//
//
// The following convenience macros are used to simplify the definition
// process for commonly specified parameters to the basic TOKEN_DEF macro.
// DEFINE_BASIC_TOKEN(name, type, ...)
// DEFINE_INDEXED_TOKEN(name, type, arraysize, ...)
// DEFINE_COUNTER_TOKEN(name, type, ...)
// DEFINE_FIXED_BASIC_TOKEN(name, type, address, ...)
// DEFINE_FIXED_INDEXED_TOKEN(name, type, arraysize, address, ...)
// DEFINE_FIXED_COUNTER_TOKEN(name, type, address, ...)
// DEFINE_MFG_TOKEN(name, type, address, ...)
//
#define DEFINE_BASIC_TOKEN(name, type, ...) \
TOKEN_DEF(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
#define DEFINE_COUNTER_TOKEN(name, type, ...) \
TOKEN_DEF(name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)
#define DEFINE_INDEXED_TOKEN(name, type, arraysize, ...) \
TOKEN_DEF(name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)
#define DEFINE_FIXED_BASIC_TOKEN(name, type, address, ...) \
TOKEN_NEXT_ADDRESS(name, (address)) \
TOKEN_DEF(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
#define DEFINE_FIXED_COUNTER_TOKEN(name, type, address, ...) \
TOKEN_NEXT_ADDRESS(name, (address)) \
TOKEN_DEF(name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)
#define DEFINE_FIXED_INDEXED_TOKEN(name, type, arraysize, address, ...) \
TOKEN_NEXT_ADDRESS(name, (address)) \
TOKEN_DEF(name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)
#define DEFINE_MFG_TOKEN(name, type, address, ...) \
TOKEN_NEXT_ADDRESS(name, (address)) \
TOKEN_MFG(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
// The Simulated EEPROM and NVM3 unit tests define their own tokens.
#if !defined(SIM_EEPROM_TEST) && !defined(NVM3_TEST)
// The creator codes are here in one list instead of next to their token
// definitions so comparison of the codes is easier. The only requirement
// on these creator definitions is that they all must be unique. A favorite
// method for picking creator codes is to use two ASCII characters
// to make the codes more memorable.
// STACK CREATORS
#define CREATOR_STACK_NVDATA_VERSION 0xFF01
#define CREATOR_STACK_BOOT_COUNTER 0xE263
#define CREATOR_STACK_NONCE_COUNTER 0xE563
#define CREATOR_STACK_ANALYSIS_REBOOT 0xE162
#define CREATOR_STACK_KEYS 0xEB79
#define CREATOR_STACK_NODE_DATA 0xEE64
#define CREATOR_STACK_CLASSIC_DATA 0xE364
#define CREATOR_STACK_ALTERNATE_KEY 0xE475
#define CREATOR_STACK_APS_FRAME_COUNTER 0xE123
#define CREATOR_STACK_TRUST_CENTER 0xE124
#define CREATOR_STACK_NETWORK_MANAGEMENT 0xE125
#define CREATOR_STACK_PARENT_INFO 0xE126
#define CREATOR_STACK_PARENT_ADDITIONAL_INFO 0xE127
#define CREATOR_STACK_MULTI_PHY_NWK_INFO 0xE128
#define CREATOR_STACK_MIN_RECEIVED_RSSI 0xE129
// MULTI-NETWORK STACK CREATORS
#define CREATOR_MULTI_NETWORK_STACK_KEYS 0xE210
#define CREATOR_MULTI_NETWORK_STACK_NODE_DATA 0xE211
#define CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEY 0xE212
#define CREATOR_MULTI_NETWORK_STACK_TRUST_CENTER 0xE213
#define CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT 0xE214
#define CREATOR_MULTI_NETWORK_STACK_PARENT_INFO 0xE215
// A temporary solution for multi-network nwk counters:
// This counter will be used on the network with index 1.
#define CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTER 0xE220
#define CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO 0xE221
// GP stack tokens.
#define CREATOR_STACK_GP_DATA 0xE258
#define CREATOR_STACK_GP_PROXY_TABLE 0xE259
#define CREATOR_STACK_GP_SINK_TABLE 0xE25A
#define CREATOR_STACK_GP_INCOMING_FC 0xE25B
#define CREATOR_STACK_GP_INCOMING_FC_IN_SINK 0xE25C
// APP CREATORS
#define CREATOR_STACK_BINDING_TABLE 0xE274
#define CREATOR_STACK_CHILD_TABLE 0xFF0D
#define CREATOR_STACK_KEY_TABLE 0xE456
#define CREATOR_STACK_CERTIFICATE_TABLE 0xE500
#define CREATOR_STACK_ZLL_DATA 0xE501
#define CREATOR_STACK_ZLL_SECURITY 0xE502
#define CREATOR_STACK_ADDITIONAL_CHILD_DATA 0xE503
// NVM3KEY domain base keys
#define NVM3KEY_DOMAIN_USER 0x00000U
#define NVM3KEY_DOMAIN_ZIGBEE 0x10000U
#define NVM3KEY_DOMAIN_COMMON 0x80000U
// STACK KEYS
#define NVM3KEY_STACK_NVDATA_VERSION (NVM3KEY_DOMAIN_ZIGBEE | 0xFF01)
#define NVM3KEY_STACK_BOOT_COUNTER (NVM3KEY_DOMAIN_ZIGBEE | 0xE263)
#define NVM3KEY_STACK_NONCE_COUNTER (NVM3KEY_DOMAIN_ZIGBEE | 0xE563)
#define NVM3KEY_STACK_ANALYSIS_REBOOT (NVM3KEY_DOMAIN_ZIGBEE | 0xE162)
#define NVM3KEY_STACK_KEYS (NVM3KEY_DOMAIN_ZIGBEE | 0xEB79)
#define NVM3KEY_STACK_NODE_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0xEE64)
#define NVM3KEY_STACK_CLASSIC_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0xE364)
#define NVM3KEY_STACK_ALTERNATE_KEY (NVM3KEY_DOMAIN_ZIGBEE | 0xE475)
#define NVM3KEY_STACK_APS_FRAME_COUNTER (NVM3KEY_DOMAIN_ZIGBEE | 0xE123)
#define NVM3KEY_STACK_TRUST_CENTER (NVM3KEY_DOMAIN_ZIGBEE | 0xE124)
#define NVM3KEY_STACK_NETWORK_MANAGEMENT (NVM3KEY_DOMAIN_ZIGBEE | 0xE125)
#define NVM3KEY_STACK_PARENT_INFO (NVM3KEY_DOMAIN_ZIGBEE | 0xE126)
#define NVM3KEY_STACK_PARENT_ADDITIONAL_INFO (NVM3KEY_DOMAIN_ZIGBEE | 0xE127)
#define NVM3KEY_STACK_MULTI_PHY_NWK_INFO (NVM3KEY_DOMAIN_ZIGBEE | 0xE128)
#define NVM3KEY_STACK_MIN_RECEIVED_RSSI (NVM3KEY_DOMAIN_ZIGBEE | 0xE129)
// MULTI-NETWORK STACK KEYS
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_KEYS (NVM3KEY_DOMAIN_ZIGBEE | 0x0000)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_NODE_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0x0080)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEY (NVM3KEY_DOMAIN_ZIGBEE | 0x0100)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTER (NVM3KEY_DOMAIN_ZIGBEE | 0x0180)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT (NVM3KEY_DOMAIN_ZIGBEE | 0x0200)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFO (NVM3KEY_DOMAIN_ZIGBEE | 0x0280)
// Temporary solution for multi-network nwk counters:
// This counter will be used on the network with index 1.
#define NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTER (NVM3KEY_DOMAIN_ZIGBEE | 0xE220)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved
#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO (NVM3KEY_DOMAIN_ZIGBEE | 0x0300)
// GP stack tokens.
#define NVM3KEY_STACK_GP_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0xE258)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_GP_PROXY_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0380)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_GP_SINK_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0400)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved
#define NVM3KEY_STACK_GP_INCOMING_FC (NVM3KEY_DOMAIN_ZIGBEE | 0x0480)
// APP KEYS
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_BINDING_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0500)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_CHILD_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0580)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_KEY_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0600)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_CERTIFICATE_TABLE (NVM3KEY_DOMAIN_ZIGBEE | 0x0680)
#define NVM3KEY_STACK_ZLL_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0xE501)
#define NVM3KEY_STACK_ZLL_SECURITY (NVM3KEY_DOMAIN_ZIGBEE | 0xE502)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved.
#define NVM3KEY_STACK_ADDITIONAL_CHILD_DATA (NVM3KEY_DOMAIN_ZIGBEE | 0x0700)
// This key is used for an indexed token and the subsequent 0x7F keys are also reserved
#define NVM3KEY_STACK_GP_INCOMING_FC_IN_SINK (NVM3KEY_DOMAIN_ZIGBEE | 0x0780)
// MANUFACTURING DATA
// Pull in the platform-specific manufacturing tokens
#if defined(CORTEXM3)
// Cortex-M3 handles MFG tokens separately via mfg-token.h.
#elif defined(EZSP_HOST) || defined(ZIGBEE_STACK_ON_HOST)
// No MFG tokens on hosts or Zigbeed.
#elif defined(EMBER_TEST)
#include "hal/micro/unix/simulation/token-manufacturing.h"
#else
#error no platform defined
#endif
// STACK DATA
// *The addresses of these tokens must not change.*
#define CURRENT_STACK_TOKEN_VERSION 0x03FC //MSB is version, LSB is complement.
#ifdef DEFINETYPES
typedef uint16_t tokTypeStackNvdataVersion;
typedef uint32_t tokTypeStackBootCounter;
//This was introduced to save the type of keep alives supported by the parent.
//Bits 0-2 are currently in use, bit 2 covers power negotiation.
//Bits 3-14 are reserved. Bit 15 is used in alt-mac
typedef uint16_t tokTypeStackParentAdditionalInfo;
typedef uint16_t tokTypeStackAnalysisReboot;
typedef uint32_t tokTypeStackNonceCounter;
typedef int8_t tokTypeRSSI;
typedef struct {
uint8_t networkKey[16];
uint8_t activeKeySeqNum;
} tokTypeStackKeys;
typedef struct {
uint16_t panId;
int8_t radioTxPower;
uint8_t radioFreqChannel;
uint8_t stackProfile;
uint8_t nodeType;
uint16_t zigbeeNodeId;
uint8_t extendedPanId[8];
} tokTypeStackNodeData;
typedef struct {
uint16_t mode;
uint8_t eui64[8];
uint8_t key[16];
} tokTypeStackTrustCenter;
typedef struct {
uint32_t activeChannels;
uint16_t managerNodeId;
uint8_t updateId;
} tokTypeStackNetworkManagement;
typedef struct {
uint8_t parentEui[8];
uint16_t parentNodeId;
} tokTypeStackParentInfo;
typedef struct {
int8_t radioTxPower;
uint8_t radioFreqChannel;
uint32_t pg28ChannelMask;
uint32_t pg29ChannelMask;
uint32_t pg30ChannelMask;
uint32_t pg31ChannelMask;
uint8_t optionsMask;
} tokTypeStackMultiPhyNwkInfo;
#endif //DEFINETYPES
#ifdef DEFINETOKENS
// The stack tokens also need to be stored at well-defined locations.
// None of these addresses should ever change without extremely great care.
#define STACK_VERSION_LOCATION 128 // 2 bytes
#define STACK_APS_NONCE_LOCATION 130 // 4 bytes
#define STACK_ALT_NWK_KEY_LOCATION 134 // 17 bytes (key + sequence number)
// reserved 151 1 bytes
#define STACK_BOOT_COUNT_LOCATION 152 // 2 bytes
// reserved 154 2 bytes
#define STACK_NONCE_LOCATION 156 // 4 bytes
// reserved 160 1 bytes
#define STACK_REBOOT_LOCATION 161 // 2 bytes
// reserved 163 7 bytes
#define STACK_KEYS_LOCATION 170 // 17 bytes
// reserved 187 5 bytes
#define STACK_NODE_DATA_LOCATION 192 // 16 bytes
#define STACK_CLASSIC_LOCATION 208 // 26 bytes
#define STACK_TRUST_CENTER_LOCATION 234 //26 bytes
// reserved 260 8 bytes
#define STACK_NETWORK_MANAGEMENT_LOCATION 268 // 7 bytes
#define STACK_PARENT_INFO_LOCATION 276 //10 bytes
#define STACK_PARENT_ADDITIONAL_INFO_LOCATION 286 //2 bytes
#define STACK_MULTI_PHY_NWK_INFO_LOCATION 288 // 19 bytes
#define STACK_MIN_RECEIVED_RSSI_LOCATION 307 // 1 byte
// reserved 308 107 bytes
DEFINE_FIXED_BASIC_TOKEN(STACK_NVDATA_VERSION,
tokTypeStackNvdataVersion,
STACK_VERSION_LOCATION,
CURRENT_STACK_TOKEN_VERSION)
DEFINE_FIXED_COUNTER_TOKEN(STACK_APS_FRAME_COUNTER,
tokTypeStackNonceCounter,
STACK_APS_NONCE_LOCATION,
0x00000000)
DEFINE_FIXED_BASIC_TOKEN(STACK_ALTERNATE_KEY,
tokTypeStackKeys,
STACK_ALT_NWK_KEY_LOCATION,
{ { 0, } })
DEFINE_FIXED_COUNTER_TOKEN(STACK_BOOT_COUNTER,
tokTypeStackBootCounter,
STACK_BOOT_COUNT_LOCATION,
0x0000)
DEFINE_FIXED_COUNTER_TOKEN(STACK_NONCE_COUNTER,
tokTypeStackNonceCounter,
STACK_NONCE_LOCATION,
0x00000000)
DEFINE_FIXED_BASIC_TOKEN(STACK_ANALYSIS_REBOOT,
tokTypeStackAnalysisReboot,
STACK_REBOOT_LOCATION,
0x0000)
DEFINE_FIXED_BASIC_TOKEN(STACK_KEYS,
tokTypeStackKeys,
STACK_KEYS_LOCATION,
{ { 0, } })
DEFINE_FIXED_BASIC_TOKEN(STACK_NODE_DATA,
tokTypeStackNodeData,
STACK_NODE_DATA_LOCATION,
{ 0xFFFF, -1, 0, 0x00, 0x00, 0x0000 })
DEFINE_FIXED_BASIC_TOKEN(STACK_TRUST_CENTER,
tokTypeStackTrustCenter,
STACK_TRUST_CENTER_LOCATION,
{ 0, })
DEFINE_FIXED_BASIC_TOKEN(STACK_NETWORK_MANAGEMENT,
tokTypeStackNetworkManagement,
STACK_NETWORK_MANAGEMENT_LOCATION,
{ 0, 0xFFFF, 0 })
DEFINE_FIXED_BASIC_TOKEN(STACK_PARENT_INFO,
tokTypeStackParentInfo,
STACK_PARENT_INFO_LOCATION,
{ { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF }, 0xFFFF })
DEFINE_FIXED_BASIC_TOKEN(STACK_PARENT_ADDITIONAL_INFO,
tokTypeStackParentAdditionalInfo,
STACK_PARENT_ADDITIONAL_INFO_LOCATION,
0x0000)
DEFINE_FIXED_BASIC_TOKEN(STACK_MULTI_PHY_NWK_INFO,
tokTypeStackMultiPhyNwkInfo,
STACK_MULTI_PHY_NWK_INFO_LOCATION,
{ -1, 0, 0, 0, 0, 0, 0x80 })
DEFINE_FIXED_BASIC_TOKEN(STACK_MIN_RECEIVED_RSSI,
tokTypeRSSI,
STACK_MIN_RECEIVED_RSSI_LOCATION,
{ -100, })
#endif //DEFINETOKENS
// PHY DATA
//
#include "token-phy.h"
// MULTI-NETWORK STACK TOKENS: Tokens for the networks with index > 0.
// The 0-index network info is stored in the usual tokens.
#ifdef DEFINETOKENS
#ifndef SMART_ENERGY_STACK_TOKENS
//#if !defined(EMBER_MULTI_NETWORK_STRIPPED)
// EMBER_MULTI_NETWORK_STRIPPED is commented out to work around
// EMZIGBEE-2676 / EMHAL-1530. This header is used somewhere
// that doesn't include ember.h, so it leads to conflicting
// definitions. Eating the extra tokens is much easier than double
// building every library that touches a token.
#define EXTRA_NETWORKS_NUMBER (EMBER_SUPPORTED_NETWORKS - 1)
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_KEYS,
tokTypeStackKeys,
EXTRA_NETWORKS_NUMBER,
{ { 0, } })
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_NODE_DATA,
tokTypeStackNodeData,
EXTRA_NETWORKS_NUMBER,
{ 0, })
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_ALTERNATE_KEY,
tokTypeStackKeys,
EXTRA_NETWORKS_NUMBER,
{ { 0, } })
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_TRUST_CENTER,
tokTypeStackTrustCenter,
EXTRA_NETWORKS_NUMBER,
{ 0, })
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_NETWORK_MANAGEMENT,
tokTypeStackNetworkManagement,
EXTRA_NETWORKS_NUMBER,
{ 0, })
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_PARENT_INFO,
tokTypeStackParentInfo,
EXTRA_NETWORKS_NUMBER,
{ { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF }, 0xFFFF })
// Temporary solution for NWK counter token: the following is used for 1-index
// network.
DEFINE_COUNTER_TOKEN(MULTI_NETWORK_STACK_NONCE_COUNTER,
tokTypeStackNonceCounter,
0x00000000)
DEFINE_INDEXED_TOKEN(MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO,
tokTypeStackParentAdditionalInfo,
EXTRA_NETWORKS_NUMBER,
{ 0, })
//#endif // EMBER_MULTI_NETWORK_STRIPPED
#endif // SMART_ENERGY_STACK_TOKENS
#endif // DEFINETOKENS
// APPLICATION DATA
// *If a fixed application token is desired, its address must be above 384.*
#ifdef DEFINETYPES
typedef uint8_t tokTypeStackBindingTable[13];
typedef uint8_t tokTypeStackChildTable[11];
typedef uint8_t tokTypeStackKeyTable[25];
typedef uint8_t tokTypeStackAdditionalChildData;
// Certificate Table Entry
// Certificate: 48-bytes
// CA Public Key: 22-bytes
// Private Key: 21-bytes
// Flags: 1-byte
#define TOKEN_CERTIFICATE_TABLE_ENTRY_SIZE (48 + 22 + 21 + 1)
#define TOKEN_CERTIFICATE_TABLE_ENTRY_FLAGS_INDEX (TOKEN_CERTIFICATE_TABLE_ENTRY_SIZE - 1)
typedef uint8_t tokTypeStackCertificateTable[TOKEN_CERTIFICATE_TABLE_ENTRY_SIZE];
#endif //DEFINETYPES
// The following application tokens are required by the stack, but are sized by
// the application via its CONFIGURATION_HEADER, which is why they are present
// within the application data section. Any special application-defined
// tokens will follow.
// NOTE: changing the size of these tokens within the CONFIGURATION_HEADER
// WILL automatically move any custom application tokens that are defined
// in the APPLICATION_TOKEN_HEADER.
#ifdef DEFINETOKENS
// Application tokens start at location 384 and are automatically positioned.
TOKEN_NEXT_ADDRESS(APP, 384)
DEFINE_INDEXED_TOKEN(STACK_BINDING_TABLE,
tokTypeStackBindingTable,
EMBER_BINDING_TABLE_SIZE,
{ 0, })
DEFINE_INDEXED_TOKEN(STACK_CHILD_TABLE,
tokTypeStackChildTable,
EMBER_CHILD_TABLE_SIZE,
{ 0, })
DEFINE_INDEXED_TOKEN(STACK_KEY_TABLE,
tokTypeStackKeyTable,
EMBER_KEY_TABLE_SIZE,
{ 0, })
DEFINE_INDEXED_TOKEN(STACK_CERTIFICATE_TABLE,
tokTypeStackCertificateTable,
EMBER_CERTIFICATE_TABLE_SIZE,
{ 0, })
DEFINE_INDEXED_TOKEN(STACK_ADDITIONAL_CHILD_DATA,
tokTypeStackAdditionalChildData,
EMBER_CHILD_TABLE_SIZE,
{ 0x0F, })
#endif //DEFINETOKENS
#ifndef SMART_ENERGY_STACK_TOKENS
// These must appear before the application header so that the token
// numbering is consistent regardless of whether application tokens are
// defined.
//#if defined(EMBER_AF_PLUGIN_ZLL_LIBRARY) || defined(EMBER_TEST)
#include "stack/zll/zll-token-config.h"
//#endif
#ifdef UC_BUILD
#if defined(SL_CATALOG_ZIGBEE_GREEN_POWER_PRESENT) || defined(EMBER_TEST)
#include "stack/gp/gp-token-config.h"
#endif // (SL_CATALOG_ZIGBEE_GREEN_POWER_PRESENT) || (EMBER_TEST)
#else // !UC_BUILD
//#if defined(EMBER_AF_PLUGIN_GP_LIBRARY) || defined(EMBER_TEST)
#include "stack/gp/gp-token-config.h"
//#endif
#endif // UC_BUILD
#include "stack/core/multi-pan-token-config.h"
#endif // SMART_ENERGY_STACK_TOKENS
#ifdef UC_BUILD
#ifdef SL_CATALOG_ZIGBEE_ZCL_FRAMEWORK_CORE_PRESENT
#include "app/framework/util/af-token.h"
#endif
#ifdef SL_CATALOG_ZIGBEE_NCP_FRAMEWORK_PRESENT
#include "app/framework/util/af-ncp-token.h"
#endif
#else
#ifdef APPLICATION_TOKEN_HEADER
#include APPLICATION_TOKEN_HEADER
#endif
#endif // UC_BUILD
//The tokens defined below are test tokens. They are normally not used
//but are left here as a convenience so test tokens do not have to
//be recreated. If test code needs temporary, non-volatile storage,
//uncomment and alter the set below as needed.
//#define CREATOR_TT01 1
//#define CREATOR_TT02 2
//#define CREATOR_TT03 3
//#define CREATOR_TT04 4
//#define CREATOR_TT05 5
//#define CREATOR_TT06 6
//#ifdef DEFINETYPES
//typedef uint32_t tokTypeTT01;
//typedef uint32_t tokTypeTT02;
//typedef uint32_t tokTypeTT03;
//typedef uint32_t tokTypeTT04;
//typedef uint16_t tokTypeTT05;
//typedef uint16_t tokTypeTT06;
//#endif //DEFINETYPES
//#ifdef DEFINETOKENS
//#define TT01_LOCATION 1
//#define TT02_LOCATION 2
//#define TT03_LOCATION 3
//#define TT04_LOCATION 4
//#define TT05_LOCATION 5
//#define TT06_LOCATION 6
//DEFINE_FIXED_BASIC_TOKEN(TT01, tokTypeTT01, TT01_LOCATION, 0x0000)
//DEFINE_FIXED_BASIC_TOKEN(TT02, tokTypeTT02, TT02_LOCATION, 0x0000)
//DEFINE_FIXED_BASIC_TOKEN(TT03, tokTypeTT03, TT03_LOCATION, 0x0000)
//DEFINE_FIXED_BASIC_TOKEN(TT04, tokTypeTT04, TT04_LOCATION, 0x0000)
//DEFINE_FIXED_BASIC_TOKEN(TT05, tokTypeTT05, TT05_LOCATION, 0x0000)
//DEFINE_FIXED_BASIC_TOKEN(TT06, tokTypeTT06, TT06_LOCATION, 0x0000)
//#endif //DEFINETOKENS
#else // !defined(SIM_EEPROM_TEST) && !defined(NVM3_TEST)
//The Simulated EEPROM and NVM3 unit tests define their tokens via the
//APPLICATION_TOKEN_HEADER macro.
#ifdef UC_BUILD
#ifdef SL_CATALOG_ZIGBEE_ZCL_FRAMEWORK_CORE_PRESENT
#include "app/framework/util/af-token.h"
#endif
#ifdef SL_CATALOG_ZIGBEE_NCP_FRAMEWORK_PRESENT
#include "app/framework/util/af-ncp-token.h"
#endif
#else
#ifdef APPLICATION_TOKEN_HEADER
#include APPLICATION_TOKEN_HEADER
#endif
#endif // UC_BUILD
#endif // !defined(SIM_EEPROM_TEST) && !defined(NVM3_TEST)
#ifndef DEFINEADDRESSES
#undef TOKEN_NEXT_ADDRESS
#endif
Convenience Macros#
The following convenience macros are used to simplify the definition process for commonly specified parameters to the basic TOKEN_DEF macro. See hal/micro/token.h for a more complete explanation.
Creator Codes#
The CREATOR is used as a distinct identifier tag for the token.The CREATOR is necessary because the token name is defined differently depending on the hardware platform. Therefore, the CREATOR ensures that token definitions and data stay tagged and known. The only requirement is that each creator definition must be unique. See hal/micro/token.h for a more complete explanation.
NVM3 Object Keys#
The NVM3 object key is used as a distinct identifier tag for a token stored in NVM3.Every token must have a defined NVM3 object key and the object key must be unique. The object key defined must be in the following format: NVM3KEY_tokennamewhere tokenname is the name of the token without NVM3KEY_ or TOKEN_ prefix.
Macros#
By default, tokens are automatically located after the previous token.
The current version number of the stack tokens. MSB is the version, LSB is a complement.
Convenience Macros Documentation#
DEFINE_BASIC_TOKEN#
#define DEFINE_BASIC_TOKENValue:
(name, type, ...)
103
of file stack/config/token-stack.h
DEFINE_COUNTER_TOKEN#
#define DEFINE_COUNTER_TOKENValue:
(name, type, ...)
106
of file stack/config/token-stack.h
DEFINE_INDEXED_TOKEN#
#define DEFINE_INDEXED_TOKENValue:
(name, type, arraysize, ...)
109
of file stack/config/token-stack.h
DEFINE_FIXED_BASIC_TOKEN#
#define DEFINE_FIXED_BASIC_TOKENValue:
112
of file stack/config/token-stack.h
DEFINE_FIXED_COUNTER_TOKEN#
#define DEFINE_FIXED_COUNTER_TOKENValue:
116
of file stack/config/token-stack.h
DEFINE_FIXED_INDEXED_TOKEN#
#define DEFINE_FIXED_INDEXED_TOKENValue:
120
of file stack/config/token-stack.h
DEFINE_MFG_TOKEN#
#define DEFINE_MFG_TOKENValue:
124
of file stack/config/token-stack.h
Creator Codes Documentation#
CREATOR_STACK_NVDATA_VERSION#
#define CREATOR_STACK_NVDATA_VERSIONValue:
0xFF01
153
of file stack/config/token-stack.h
CREATOR_STACK_BOOT_COUNTER#
#define CREATOR_STACK_BOOT_COUNTERValue:
0xE263
154
of file stack/config/token-stack.h
CREATOR_STACK_NONCE_COUNTER#
#define CREATOR_STACK_NONCE_COUNTERValue:
0xE563
155
of file stack/config/token-stack.h
CREATOR_STACK_ANALYSIS_REBOOT#
#define CREATOR_STACK_ANALYSIS_REBOOTValue:
0xE162
156
of file stack/config/token-stack.h
CREATOR_STACK_KEYS#
#define CREATOR_STACK_KEYSValue:
0xEB79
157
of file stack/config/token-stack.h
CREATOR_STACK_NODE_DATA#
#define CREATOR_STACK_NODE_DATAValue:
0xEE64
158
of file stack/config/token-stack.h
CREATOR_STACK_CLASSIC_DATA#
#define CREATOR_STACK_CLASSIC_DATAValue:
0xE364
159
of file stack/config/token-stack.h
CREATOR_STACK_ALTERNATE_KEY#
#define CREATOR_STACK_ALTERNATE_KEYValue:
0xE475
160
of file stack/config/token-stack.h
CREATOR_STACK_APS_FRAME_COUNTER#
#define CREATOR_STACK_APS_FRAME_COUNTERValue:
0xE123
161
of file stack/config/token-stack.h
CREATOR_STACK_TRUST_CENTER#
#define CREATOR_STACK_TRUST_CENTERValue:
0xE124
162
of file stack/config/token-stack.h
CREATOR_STACK_NETWORK_MANAGEMENT#
#define CREATOR_STACK_NETWORK_MANAGEMENTValue:
0xE125
163
of file stack/config/token-stack.h
CREATOR_STACK_PARENT_INFO#
#define CREATOR_STACK_PARENT_INFOValue:
0xE126
164
of file stack/config/token-stack.h
CREATOR_STACK_PARENT_ADDITIONAL_INFO#
#define CREATOR_STACK_PARENT_ADDITIONAL_INFOValue:
0xE127
165
of file stack/config/token-stack.h
CREATOR_STACK_MULTI_PHY_NWK_INFO#
#define CREATOR_STACK_MULTI_PHY_NWK_INFOValue:
0xE128
166
of file stack/config/token-stack.h
CREATOR_STACK_MIN_RECEIVED_RSSI#
#define CREATOR_STACK_MIN_RECEIVED_RSSIValue:
0xE129
167
of file stack/config/token-stack.h
CREATOR_MULTI_NETWORK_STACK_KEYS#
#define CREATOR_MULTI_NETWORK_STACK_KEYSValue:
0xE210
169
of file stack/config/token-stack.h
CREATOR_MULTI_NETWORK_STACK_NODE_DATA#
#define CREATOR_MULTI_NETWORK_STACK_NODE_DATAValue:
0xE211
170
of file stack/config/token-stack.h
CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEY#
#define CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEYValue:
0xE212
171
of file stack/config/token-stack.h
CREATOR_MULTI_NETWORK_STACK_TRUST_CENTER#
#define CREATOR_MULTI_NETWORK_STACK_TRUST_CENTERValue:
0xE213
172
of file stack/config/token-stack.h
CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT#
#define CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENTValue:
0xE214
173
of file stack/config/token-stack.h
CREATOR_MULTI_NETWORK_STACK_PARENT_INFO#
#define CREATOR_MULTI_NETWORK_STACK_PARENT_INFOValue:
0xE215
174
of file stack/config/token-stack.h
CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTER#
#define CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTERValue:
0xE220
178
of file stack/config/token-stack.h
CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO#
#define CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFOValue:
0xE221
179
of file stack/config/token-stack.h
CREATOR_STACK_GP_DATA#
#define CREATOR_STACK_GP_DATAValue:
0xE258
182
of file stack/config/token-stack.h
CREATOR_STACK_GP_PROXY_TABLE#
#define CREATOR_STACK_GP_PROXY_TABLEValue:
0xE259
183
of file stack/config/token-stack.h
CREATOR_STACK_GP_SINK_TABLE#
#define CREATOR_STACK_GP_SINK_TABLEValue:
0xE25A
184
of file stack/config/token-stack.h
CREATOR_STACK_GP_INCOMING_FC#
#define CREATOR_STACK_GP_INCOMING_FCValue:
0xE25B
185
of file stack/config/token-stack.h
CREATOR_STACK_GP_INCOMING_FC_IN_SINK#
#define CREATOR_STACK_GP_INCOMING_FC_IN_SINKValue:
0xE25C
186
of file stack/config/token-stack.h
CREATOR_STACK_BINDING_TABLE#
#define CREATOR_STACK_BINDING_TABLEValue:
0xE274
188
of file stack/config/token-stack.h
CREATOR_STACK_CHILD_TABLE#
#define CREATOR_STACK_CHILD_TABLEValue:
0xFF0D
189
of file stack/config/token-stack.h
CREATOR_STACK_KEY_TABLE#
#define CREATOR_STACK_KEY_TABLEValue:
0xE456
190
of file stack/config/token-stack.h
CREATOR_STACK_CERTIFICATE_TABLE#
#define CREATOR_STACK_CERTIFICATE_TABLEValue:
0xE500
191
of file stack/config/token-stack.h
CREATOR_STACK_ZLL_DATA#
#define CREATOR_STACK_ZLL_DATAValue:
0xE501
192
of file stack/config/token-stack.h
CREATOR_STACK_ZLL_SECURITY#
#define CREATOR_STACK_ZLL_SECURITYValue:
0xE502
193
of file stack/config/token-stack.h
CREATOR_STACK_ADDITIONAL_CHILD_DATA#
#define CREATOR_STACK_ADDITIONAL_CHILD_DATAValue:
0xE503
194
of file stack/config/token-stack.h
NVM3 Object Keys Documentation#
NVM3KEY_DOMAIN_USER#
#define NVM3KEY_DOMAIN_USERValue:
0x00000U
215
of file stack/config/token-stack.h
NVM3KEY_DOMAIN_ZIGBEE#
#define NVM3KEY_DOMAIN_ZIGBEEValue:
0x10000U
216
of file stack/config/token-stack.h
NVM3KEY_DOMAIN_COMMON#
#define NVM3KEY_DOMAIN_COMMONValue:
0x80000U
217
of file stack/config/token-stack.h
NVM3KEY_STACK_NVDATA_VERSION#
#define NVM3KEY_STACK_NVDATA_VERSIONValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xFF01)
220
of file stack/config/token-stack.h
NVM3KEY_STACK_BOOT_COUNTER#
#define NVM3KEY_STACK_BOOT_COUNTERValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE263)
221
of file stack/config/token-stack.h
NVM3KEY_STACK_NONCE_COUNTER#
#define NVM3KEY_STACK_NONCE_COUNTERValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE563)
222
of file stack/config/token-stack.h
NVM3KEY_STACK_ANALYSIS_REBOOT#
#define NVM3KEY_STACK_ANALYSIS_REBOOTValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE162)
223
of file stack/config/token-stack.h
NVM3KEY_STACK_KEYS#
#define NVM3KEY_STACK_KEYSValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xEB79)
224
of file stack/config/token-stack.h
NVM3KEY_STACK_NODE_DATA#
#define NVM3KEY_STACK_NODE_DATAValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xEE64)
225
of file stack/config/token-stack.h
NVM3KEY_STACK_CLASSIC_DATA#
#define NVM3KEY_STACK_CLASSIC_DATAValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE364)
226
of file stack/config/token-stack.h
NVM3KEY_STACK_ALTERNATE_KEY#
#define NVM3KEY_STACK_ALTERNATE_KEYValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE475)
227
of file stack/config/token-stack.h
NVM3KEY_STACK_APS_FRAME_COUNTER#
#define NVM3KEY_STACK_APS_FRAME_COUNTERValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE123)
228
of file stack/config/token-stack.h
NVM3KEY_STACK_TRUST_CENTER#
#define NVM3KEY_STACK_TRUST_CENTERValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE124)
229
of file stack/config/token-stack.h
NVM3KEY_STACK_NETWORK_MANAGEMENT#
#define NVM3KEY_STACK_NETWORK_MANAGEMENTValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE125)
230
of file stack/config/token-stack.h
NVM3KEY_STACK_PARENT_INFO#
#define NVM3KEY_STACK_PARENT_INFOValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE126)
231
of file stack/config/token-stack.h
NVM3KEY_STACK_PARENT_ADDITIONAL_INFO#
#define NVM3KEY_STACK_PARENT_ADDITIONAL_INFOValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE127)
232
of file stack/config/token-stack.h
NVM3KEY_STACK_MULTI_PHY_NWK_INFO#
#define NVM3KEY_STACK_MULTI_PHY_NWK_INFOValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE128)
233
of file stack/config/token-stack.h
NVM3KEY_STACK_MIN_RECEIVED_RSSI#
#define NVM3KEY_STACK_MIN_RECEIVED_RSSIValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE129)
234
of file stack/config/token-stack.h
NVM3KEY_MULTI_NETWORK_STACK_KEYS#
#define NVM3KEY_MULTI_NETWORK_STACK_KEYSValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0000)
237
of file stack/config/token-stack.h
NVM3KEY_MULTI_NETWORK_STACK_NODE_DATA#
#define NVM3KEY_MULTI_NETWORK_STACK_NODE_DATAValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0080)
239
of file stack/config/token-stack.h
NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEY#
#define NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEYValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0100)
241
of file stack/config/token-stack.h
NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTER#
#define NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTERValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0180)
243
of file stack/config/token-stack.h
NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT#
#define NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENTValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0200)
245
of file stack/config/token-stack.h
NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFO#
#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFOValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0280)
247
of file stack/config/token-stack.h
NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTER#
#define NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTERValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE220)
251
of file stack/config/token-stack.h
NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO#
#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFOValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0300)
253
of file stack/config/token-stack.h
NVM3KEY_STACK_GP_DATA#
#define NVM3KEY_STACK_GP_DATAValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE258)
256
of file stack/config/token-stack.h
NVM3KEY_STACK_GP_PROXY_TABLE#
#define NVM3KEY_STACK_GP_PROXY_TABLEValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0380)
258
of file stack/config/token-stack.h
NVM3KEY_STACK_GP_SINK_TABLE#
#define NVM3KEY_STACK_GP_SINK_TABLEValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0400)
260
of file stack/config/token-stack.h
NVM3KEY_STACK_GP_INCOMING_FC#
#define NVM3KEY_STACK_GP_INCOMING_FCValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0480)
262
of file stack/config/token-stack.h
NVM3KEY_STACK_BINDING_TABLE#
#define NVM3KEY_STACK_BINDING_TABLEValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0500)
266
of file stack/config/token-stack.h
NVM3KEY_STACK_CHILD_TABLE#
#define NVM3KEY_STACK_CHILD_TABLEValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0580)
268
of file stack/config/token-stack.h
NVM3KEY_STACK_KEY_TABLE#
#define NVM3KEY_STACK_KEY_TABLEValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0600)
270
of file stack/config/token-stack.h
NVM3KEY_STACK_CERTIFICATE_TABLE#
#define NVM3KEY_STACK_CERTIFICATE_TABLEValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0680)
272
of file stack/config/token-stack.h
NVM3KEY_STACK_ZLL_DATA#
#define NVM3KEY_STACK_ZLL_DATAValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE501)
273
of file stack/config/token-stack.h
NVM3KEY_STACK_ZLL_SECURITY#
#define NVM3KEY_STACK_ZLL_SECURITYValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE502)
274
of file stack/config/token-stack.h
NVM3KEY_STACK_ADDITIONAL_CHILD_DATA#
#define NVM3KEY_STACK_ADDITIONAL_CHILD_DATAValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0700)
276
of file stack/config/token-stack.h
NVM3KEY_STACK_GP_INCOMING_FC_IN_SINK#
#define NVM3KEY_STACK_GP_INCOMING_FC_IN_SINKValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0780)
279
of file stack/config/token-stack.h
Macro Definition Documentation#
TOKEN_NEXT_ADDRESS#
#define TOKEN_NEXT_ADDRESS
By default, tokens are automatically located after the previous token.
If a token needs to be placed at a specific location, one of the DEFINE_FIXED_* definitions should be used. This macro is inherently used in the DEFINE_FIXED_* definition to locate a token and under special circumstances (such as manufacturing tokens) it may be explicitly used.
67
of file stack/config/token-stack.h
CURRENT_STACK_TOKEN_VERSION#
#define CURRENT_STACK_TOKEN_VERSIONValue:
0x03FC
The current version number of the stack tokens. MSB is the version, LSB is a complement.
See hal/micro/token.h for a more complete explanation.
305
of file stack/config/token-stack.h