Modules#

EmberZllSecurityAlgorithmData

EmberZllNetwork

EmberZllDeviceInfoRecord

EmberZllAddressAssignment

EmberZllInitialSecurityState

EmberTokTypeStackZllData

EmberTokTypeStackZllSecurity

Ember data type definitions.

See Ember ZigBee Light Link (ZLL) Data Types for details.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

/***************************************************************************/
#ifndef SILABS_ZLL_TYPES_H
#define SILABS_ZLL_TYPES_H


#define EMBER_ZLL_PRIMARY_CHANNEL_MASK ((uint32_t)(BIT32(11)   \
                                                   | BIT32(15) \
                                                   | BIT32(20) \
                                                   | BIT32(25)))

#define EMBER_ZLL_SECONDARY_CHANNEL_MASK ((uint32_t)(BIT32(12)   \
                                                     | BIT32(13) \
                                                     | BIT32(14) \
                                                     | BIT32(16) \
                                                     | BIT32(17) \
                                                     | BIT32(18) \
                                                     | BIT32(19) \
                                                     | BIT32(21) \
                                                     | BIT32(22) \
                                                     | BIT32(23) \
                                                     | BIT32(24) \
                                                     | BIT32(26)))

#define EMBER_ZLL_NULL_NODE_ID 0x0000

#define EMBER_ZLL_MIN_NODE_ID 0x0001

#define EMBER_ZLL_MAX_NODE_ID 0xFFF7

#define EMBER_ZLL_NULL_GROUP_ID 0x0000

#define EMBER_ZLL_MIN_GROUP_ID 0x0001

#define EMBER_ZLL_MAX_GROUP_ID 0xFEFF

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberZllState
#else
typedef uint16_t EmberZllState;
enum
#endif
{
  EMBER_ZLL_STATE_NONE                       = 0x0000,
  EMBER_ZLL_STATE_FACTORY_NEW                = 0x0001,
  EMBER_ZLL_STATE_ADDRESS_ASSIGNMENT_CAPABLE = 0x0002,
  EMBER_ZLL_STATE_LINK_INITIATOR             = 0x0010,
  EMBER_ZLL_STATE_LINK_PRIORITY_REQUEST      = 0x0020,
  EMBER_ZLL_STATE_PROFILE_INTEROP            = 0x0080,
  EMBER_ZLL_STATE_NON_ZLL_NETWORK            = 0x0100,
};

typedef struct {
  uint32_t transactionId;
  uint32_t responseId;
  uint16_t bitmask;
} EmberZllSecurityAlgorithmData;

typedef struct {
  EmberZigbeeNetwork zigbeeNetwork;
  EmberZllSecurityAlgorithmData securityAlgorithm;
  EmberEUI64 eui64;
  EmberNodeId nodeId;
  EmberZllState state;
  EmberNodeType nodeType;
  uint8_t numberSubDevices;
  uint8_t totalGroupIdentifiers;
  uint8_t rssiCorrection;
} EmberZllNetwork;

typedef struct {
  EmberEUI64 ieeeAddress;
  uint8_t endpointId;
  uint16_t profileId;
  uint16_t deviceId;
  uint8_t version;
  uint8_t groupIdCount;
} EmberZllDeviceInfoRecord;

typedef struct {
  EmberNodeId nodeId;
  EmberNodeId freeNodeIdMin;
  EmberNodeId freeNodeIdMax;
  EmberMulticastId groupIdMin;
  EmberMulticastId groupIdMax;
  EmberMulticastId freeGroupIdMin;
  EmberMulticastId freeGroupIdMax;
} EmberZllAddressAssignment;

#define EMBER_ZLL_CLUSTER_ID 0x1000

#define EMBER_ZLL_PROFILE_ID 0xC05E

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberZllKeyIndex
#else
typedef uint8_t EmberZllKeyIndex;
enum
#endif
{
  EMBER_ZLL_KEY_INDEX_DEVELOPMENT   = 0x00,
  EMBER_ZLL_KEY_INDEX_MASTER        = 0x04,
  EMBER_ZLL_KEY_INDEX_CERTIFICATION = 0x0F,
};

#define EMBER_ZLL_KEY_MASK_DEVELOPMENT (1 << EMBER_ZLL_KEY_INDEX_DEVELOPMENT)

#define EMBER_ZLL_KEY_MASK_MASTER (1 << EMBER_ZLL_KEY_INDEX_MASTER)

#define EMBER_ZLL_KEY_MASK_CERTIFICATION (1 << EMBER_ZLL_KEY_INDEX_CERTIFICATION)

#define EMBER_ZLL_CERTIFICATION_ENCRYPTION_KEY      \
  { 0xC0, 0xC1, 0xC2, 0xC3, 0xC4, 0xC5, 0xC6, 0xC7, \
    0xC8, 0xC9, 0xCA, 0xCB, 0xCC, 0xCD, 0xCE, 0xCF }

#define EMBER_ZLL_CERTIFICATION_PRECONFIGURED_LINK_KEY \
  { 0xD0, 0xD1, 0xD2, 0xD3, 0xD4, 0xD5, 0xD6, 0xD7,    \
    0xD8, 0xD9, 0xDA, 0xDB, 0xDC, 0xDD, 0xDE, 0xDF }

typedef struct {
  uint32_t bitmask;
  EmberZllKeyIndex keyIndex;
  EmberKeyData encryptionKey;
  EmberKeyData preconfiguredKey;
} EmberZllInitialSecurityState;

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberZllPolicy
#else
typedef uint8_t EmberZllPolicy;
enum
#endif
{
  EMBER_ZLL_POLICY_DISABLED = 0x00,
  EMBER_ZLL_POLICY_ENABLED = 0x01,
  EMBER_ZLL_POLICY_TARGET = 0x02,
  EMBER_ZLL_POLICY_STEALING_ENABLED = 0x04,
  EMBER_ZLL_POLICY_REMOTE_RESET_ENABLED = 0x08,
};


typedef struct {
  uint32_t bitmask;
  uint16_t freeNodeIdMin;
  uint16_t freeNodeIdMax;
  uint16_t myGroupIdMin;
  uint16_t freeGroupIdMin;
  uint16_t freeGroupIdMax;
  uint8_t rssiCorrection;
} EmberTokTypeStackZllData;

typedef struct {
  uint32_t bitmask;
  uint8_t keyIndex;
  uint8_t encryptionKey[EMBER_ENCRYPTION_KEY_SIZE];
  uint8_t preconfiguredKey[EMBER_ENCRYPTION_KEY_SIZE];
} EmberTokTypeStackZllSecurity;

#endif // SILABS_ZLL_TYPES_H

ZigBee Light Link Types#

#define

The list of primary ZLL channels.

#define

The list of secondary ZLL channels.

#define

A distinguished network identifier in the ZLL network address space that indicates no free network identifiers were assigned to the device.

#define

The minimum network identifier in the ZLL network address space.

#define

The maximum network identifier in the ZLL network address space.

#define

A distinguished group identifier in the ZLL group address space that indicates no free group identifiers were assigned to the device.

#define

The minimum group identifier in the ZLL group address space.

#define

The maximum group identifier in the ZLL group address space.

#define

The ZigBee Light Link Commissioning cluster ID.

#define

The ZigBee Light Link Profile ID.

#define
EMBER_ZLL_KEY_MASK_DEVELOPMENT (1 << EMBER_ZLL_KEY_INDEX_DEVELOPMENT)

The key encryption bitmask corresponding to encryption key index EMBER_ZLL_KEY_INDEX_DEVELOPMENT.

#define
EMBER_ZLL_KEY_MASK_MASTER (1 << EMBER_ZLL_KEY_INDEX_MASTER)

The key encryption bitmask corresponding to encryption key index EMBER_ZLL_KEY_INDEX_MASTER.

#define
EMBER_ZLL_KEY_MASK_CERTIFICATION (1 << EMBER_ZLL_KEY_INDEX_CERTIFICATION)

THe key encryption bitmask corresponding to encryption key index EMBER_ZLL_KEY_INDEX_CERTIFICATION.

#define

The encryption key for use during development and certification in conjunction with EMBER_ZLL_KEY_INDEX_CERTIFICATION.

#define

The pre-configured link key for use during development and certification in conjunction with EMBER_ZLL_KEY_INDEX_CERTIFICATION.

enum
EMBER_ZLL_STATE_NONE = 0x0000
EMBER_ZLL_STATE_FACTORY_NEW = 0x0001
EMBER_ZLL_STATE_ADDRESS_ASSIGNMENT_CAPABLE = 0x0002
EMBER_ZLL_STATE_LINK_INITIATOR = 0x0010
EMBER_ZLL_STATE_LINK_PRIORITY_REQUEST = 0x0020
EMBER_ZLL_STATE_PROFILE_INTEROP = 0x0080
EMBER_ZLL_STATE_NON_ZLL_NETWORK = 0x0100
}

A bitmask indicating the state of the ZLL device. This maps directly to the ZLL information field in the scan response.

enum
EMBER_ZLL_KEY_INDEX_DEVELOPMENT = 0x00
EMBER_ZLL_KEY_INDEX_MASTER = 0x04
EMBER_ZLL_KEY_INDEX_CERTIFICATION = 0x0F
}

The key encryption algorithms supported by the stack.

enum
EMBER_ZLL_POLICY_DISABLED = 0x00
EMBER_ZLL_POLICY_ENABLED = 0x01
EMBER_ZLL_POLICY_TARGET = 0x02
EMBER_ZLL_POLICY_STEALING_ENABLED = 0x04
EMBER_ZLL_POLICY_REMOTE_RESET_ENABLED = 0x08
}

This enumeration indicates whether or not the stack processes ZLL messages.

ZigBee Light Link Types Documentation#

EMBER_ZLL_PRIMARY_CHANNEL_MASK#

#define EMBER_ZLL_PRIMARY_CHANNEL_MASK
Value:
((uint32_t)(BIT32(11) \
| BIT32(15) \
| BIT32(20) \
| BIT32(25)))

The list of primary ZLL channels.


Definition at line 38 of file stack/include/zll-types.h

EMBER_ZLL_SECONDARY_CHANNEL_MASK#

#define EMBER_ZLL_SECONDARY_CHANNEL_MASK
Value:
((uint32_t)(BIT32(12) \
| BIT32(13) \
| BIT32(14) \
| BIT32(16) \
| BIT32(17) \
| BIT32(18) \
| BIT32(19) \
| BIT32(21) \
| BIT32(22) \
| BIT32(23) \
| BIT32(24) \
| BIT32(26)))

The list of secondary ZLL channels.


Definition at line 46 of file stack/include/zll-types.h

EMBER_ZLL_NULL_NODE_ID#

#define EMBER_ZLL_NULL_NODE_ID
Value:
0x0000

A distinguished network identifier in the ZLL network address space that indicates no free network identifiers were assigned to the device.


Definition at line 63 of file stack/include/zll-types.h

EMBER_ZLL_MIN_NODE_ID#

#define EMBER_ZLL_MIN_NODE_ID
Value:
0x0001

The minimum network identifier in the ZLL network address space.


Definition at line 68 of file stack/include/zll-types.h

EMBER_ZLL_MAX_NODE_ID#

#define EMBER_ZLL_MAX_NODE_ID
Value:
0xFFF7

The maximum network identifier in the ZLL network address space.


Definition at line 73 of file stack/include/zll-types.h

EMBER_ZLL_NULL_GROUP_ID#

#define EMBER_ZLL_NULL_GROUP_ID
Value:
0x0000

A distinguished group identifier in the ZLL group address space that indicates no free group identifiers were assigned to the device.


Definition at line 79 of file stack/include/zll-types.h

EMBER_ZLL_MIN_GROUP_ID#

#define EMBER_ZLL_MIN_GROUP_ID
Value:
0x0001

The minimum group identifier in the ZLL group address space.


Definition at line 84 of file stack/include/zll-types.h

EMBER_ZLL_MAX_GROUP_ID#

#define EMBER_ZLL_MAX_GROUP_ID
Value:
0xFEFF

The maximum group identifier in the ZLL group address space.


Definition at line 89 of file stack/include/zll-types.h

EMBER_ZLL_CLUSTER_ID#

#define EMBER_ZLL_CLUSTER_ID
Value:
0x1000

The ZigBee Light Link Commissioning cluster ID.


Definition at line 173 of file stack/include/zll-types.h

EMBER_ZLL_PROFILE_ID#

#define EMBER_ZLL_PROFILE_ID
Value:
0xC05E

The ZigBee Light Link Profile ID.


Definition at line 178 of file stack/include/zll-types.h

EMBER_ZLL_KEY_MASK_DEVELOPMENT#

#define EMBER_ZLL_KEY_MASK_DEVELOPMENT
Value:
(1 << EMBER_ZLL_KEY_INDEX_DEVELOPMENT)

The key encryption bitmask corresponding to encryption key index EMBER_ZLL_KEY_INDEX_DEVELOPMENT.


Definition at line 202 of file stack/include/zll-types.h

EMBER_ZLL_KEY_MASK_MASTER#

#define EMBER_ZLL_KEY_MASK_MASTER
Value:
(1 << EMBER_ZLL_KEY_INDEX_MASTER)

The key encryption bitmask corresponding to encryption key index EMBER_ZLL_KEY_INDEX_MASTER.


Definition at line 208 of file stack/include/zll-types.h

EMBER_ZLL_KEY_MASK_CERTIFICATION#

#define EMBER_ZLL_KEY_MASK_CERTIFICATION
Value:
(1 << EMBER_ZLL_KEY_INDEX_CERTIFICATION)

THe key encryption bitmask corresponding to encryption key index EMBER_ZLL_KEY_INDEX_CERTIFICATION.


Definition at line 214 of file stack/include/zll-types.h

EMBER_ZLL_CERTIFICATION_ENCRYPTION_KEY#

#define EMBER_ZLL_CERTIFICATION_ENCRYPTION_KEY
Value:
{ 0xC0, 0xC1, 0xC2, 0xC3, 0xC4, 0xC5, 0xC6, 0xC7, \
0xC8, 0xC9, 0xCA, 0xCB, 0xCC, 0xCD, 0xCE, 0xCF }

The encryption key for use during development and certification in conjunction with EMBER_ZLL_KEY_INDEX_CERTIFICATION.


Definition at line 220 of file stack/include/zll-types.h

EMBER_ZLL_CERTIFICATION_PRECONFIGURED_LINK_KEY#

#define EMBER_ZLL_CERTIFICATION_PRECONFIGURED_LINK_KEY
Value:
{ 0xD0, 0xD1, 0xD2, 0xD3, 0xD4, 0xD5, 0xD6, 0xD7, \
0xD8, 0xD9, 0xDA, 0xDB, 0xDC, 0xDD, 0xDE, 0xDF }

The pre-configured link key for use during development and certification in conjunction with EMBER_ZLL_KEY_INDEX_CERTIFICATION.


Definition at line 228 of file stack/include/zll-types.h

EmberZllState#

EmberZllState

A bitmask indicating the state of the ZLL device. This maps directly to the ZLL information field in the scan response.

Enumerator
EMBER_ZLL_STATE_NONE

No state.

EMBER_ZLL_STATE_FACTORY_NEW

The device is factory new.

EMBER_ZLL_STATE_ADDRESS_ASSIGNMENT_CAPABLE

The device is capable of assigning addresses to other devices.

EMBER_ZLL_STATE_LINK_INITIATOR

The device is initiating a link operation.

EMBER_ZLL_STATE_LINK_PRIORITY_REQUEST

The device is requesting link priority.

EMBER_ZLL_STATE_PROFILE_INTEROP

The device is a ZigBee 3.0 device.

EMBER_ZLL_STATE_NON_ZLL_NETWORK

The device is on a non-ZLL network.


Definition at line 96 of file stack/include/zll-types.h

EmberZllKeyIndex#

EmberZllKeyIndex

The key encryption algorithms supported by the stack.

Enumerator
EMBER_ZLL_KEY_INDEX_DEVELOPMENT

The key encryption algorithm for use during development.

EMBER_ZLL_KEY_INDEX_MASTER

The key encryption algorithm shared by all certified devices.

EMBER_ZLL_KEY_INDEX_CERTIFICATION

The key encryption algorithm for use during development and certification.


Definition at line 184 of file stack/include/zll-types.h

EmberZllPolicy#

EmberZllPolicy

This enumeration indicates whether or not the stack processes ZLL messages.

Enumerator
EMBER_ZLL_POLICY_DISABLED

Initial state - all touchlinking is disabled.

EMBER_ZLL_POLICY_ENABLED

Indicates that ZLL processing is enabled.

EMBER_ZLL_POLICY_TARGET

Indicates that ZLL target is enabled.

EMBER_ZLL_POLICY_STEALING_ENABLED

Indicates that stealing and network update are enabled for non factory new devices.

EMBER_ZLL_POLICY_REMOTE_RESET_ENABLED

Indicates that remote reset is enabled for non factory new devices.


Definition at line 251 of file stack/include/zll-types.h