Multi-Network Manager#

EMBER_MULTI_NETWORK_STRIPPED is an optional #define that is used on flash-space constrained chips to conditionally compile out multi-network related source code.

Functions#

uint8_t

Returns the current network index.

emberSetCurrentNetwork(uint8_t index)

Sets the current network.

uint8_t

Can only be called inside an application callback.

Function Documentation#

emberGetCurrentNetwork#

uint8_t emberGetCurrentNetwork (void )

Returns the current network index.

Parameters
TypeDirectionArgument NameDescription
voidN/A

emberSetCurrentNetwork#

EmberStatus emberSetCurrentNetwork (uint8_t index)

Sets the current network.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aindex

The network index.

Returns


emberGetCallbackNetwork#

uint8_t emberGetCallbackNetwork (void )

Can only be called inside an application callback.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • the index of the network the callback refers to. If this function is called outside of a callback, it returns 0xFF.