Zigbee Event Logger APIs#

This file describes functionality for the Zigbee Event Logger feature. This feature is used to record salient events in the stack and application layer. The system event data is stored in a buffer, with hooks for the application to print and decode the logged data.

See zigbee-event-logger-gen.h for source code.

Enumerations#

enum
EMBER_LOGGER_ZIGBEE_BOOT_EVENT_ID = 0
EMBER_LOGGER_ZIGBEE_JOIN_NETWORK_ID = 1
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_REJOIN_ID = 2
EMBER_LOGGER_ZIGBEE_SECURE_REJOIN_ID = 3
EMBER_LOGGER_ZIGBEE_LEAVE_WITHOUT_REJOIN_ID = 4
EMBER_LOGGER_ZIGBEE_LEAVE_WITH_REJOIN_ID = 5
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_LINK_KEY_CHANGE_ID = 6
EMBER_LOGGER_ZIGBEE_NETWORK_KEY_SEQUENCE_NUMBER_CHANGE_ID = 7
EMBER_LOGGER_ZIGBEE_RESET_ID = 8
EMBER_LOGGER_ZIGBEE_CHANNEL_CHANGE_ID = 9
EMBER_LOGGER_ZIGBEE_PARENT_CHANGE_ID = 10
EMBER_LOGGER_ZIGBEE_DUTY_CYCLE_CHANGE_ID = 11
EMBER_LOGGER_ZIGBEE_CHILD_ADDED_ID = 12
EMBER_LOGGER_ZIGBEE_CHILD_REMOVED_ID = 13
EMBER_LOGGER_ZIGBEE_CHILD_TIMED_OUT_ID = 14
EMBER_LOGGER_ZIGBEE_STACK_STATUS_ID = 15
EMBER_LOGGER_ZIGBEE_TIME_SYNC_ID = 16
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_JOIN_DECISION_ID = 17
EMBER_LOGGER_ZIGBEE_NULL_ID = 0xFFFF
}

A list of identifiers for system events.

enum
EMBER_LOGGER_ZIGBEE_FACILITY_BASE = 0
EMBER_LOGGER_ZIGBEE_FACILITY_MAC = 1
EMBER_LOGGER_ZIGBEE_FACILITY_NETWORK = 2
EMBER_LOGGER_ZIGBEE_FACILITY_APS = 3
EMBER_LOGGER_ZIGBEE_FACILITY_SECURITY = 4
EMBER_LOGGER_ZIGBEE_FACILITY_ZDO = 5
EMBER_LOGGER_ZIGBEE_FACILITY_ZCL = 6
EMBER_LOGGER_ZIGBEE_FACILITY_BDB = 7
EMBER_LOGGER_ZIGBEE_FACILITY_SMART_ENERGY = 8
}

A list of facilities for system events, identifying which layer they occurred in.

Functions#

void
emberAfPluginZigBeeEventLoggerAddBootEvent(uint32_t bootCount, uint16_t resetType)

Record an event indicating that the device has booted.

void
emberAfPluginZigBeeEventLoggerAddJoinNetwork(EmberPanId panId, uint8_t channelNumber, uint8_t page, uint8_t *extendedPanId)

Record an event indicating that a network was successfully joined.

void
emberAfPluginZigBeeEventLoggerAddTrustCenterRejoin(uint32_t channelMask, EmberRejoinReason reason)

Record an event indicating that a trust center rejoin was attempted.

void
emberAfPluginZigBeeEventLoggerAddSecureRejoin(uint32_t channelMask, EmberRejoinReason reason)

Record an event indicating that a secure rejoin was attempted.

void
emberAfPluginZigBeeEventLoggerAddLeaveWithoutRejoin(EmberNodeId sourceNode, EmberLeaveReason reason)

Record an event indicating that a device has left-without-rejoin.

void
emberAfPluginZigBeeEventLoggerAddLeaveWithRejoin(EmberNodeId sourceNode, EmberLeaveReason reason)

Record an event indicating that a device has left-with-rejoin.

void

Record an event indicating that an attempt was made to update the trust center link key.

void

Record an event indicating that the network key sequence number has changed.

void
emberAfPluginZigBeeEventLoggerAddReset(uint8_t resetCode, uint8_t extendedReason)

Record an event indicating that the local device has reset.

void
emberAfPluginZigBeeEventLoggerAddChannelChange(uint8_t page, uint8_t channel)

Record an event indicating that the network's channel has changed.

void
emberAfPluginZigBeeEventLoggerAddParentChange(EmberNodeId parentNodeId, EmberEUI64 parentEui64)

Record an event indicating that the local device's parent has changed.

void
emberAfPluginZigBeeEventLoggerAddDutyCycleChange(EmberDutyCycleState state, EmberDutyCycleHectoPct limitThreshold, EmberDutyCycleHectoPct criticalThreshold, EmberDutyCycleHectoPct suspendedLimit)

Record an event indicating that the duty cycle has changed.

void
emberAfPluginZigBeeEventLoggerAddChildAdded(EmberNodeId childNodeId, EmberEUI64 childEui64)

Record an event indicating that a child device has joined the local device.

void
emberAfPluginZigBeeEventLoggerAddChildRemoved(EmberNodeId childNodeId, EmberEUI64 childEui64)

Record an event indicating that a child device has been removed from the local device.

void
emberAfPluginZigBeeEventLoggerAddChildTimedOut(EmberNodeId childNodeId, EmberEUI64 childEui64)

Record an event indicating that a child device has been timed out by the local device.

void

Record an event indicating that the stack status has changed.

void
emberAfPluginZigBeeEventLoggerAddTimeSync(uint32_t utcTime, uint32_t secondsSinceBoot)

Record an event indicating that the clock time has been synchronized.

void
emberAfPluginZigBeeEventLoggerAddTrustCenterJoinDecision(EmberNodeId nodeId, uint8_t decision)

Record an event indicating that a device has attempted to join or rejoin the network.

Macros#

#define
ZIGBEE_EVENT_LOGGER_VERSION 1

The version of this feature.

#define
LOGGER_AREA_BIT_SHIFT 12
#define
EMBER_ZIGBEE_LOGGER_AREA (0 << LOGGER_AREA_BIT_SHIFT)
#define
EMBER_LOGGER_ZIGBEE_BOOT_EVENT_LENGTH 6

The length of the Boot Event event data.

#define
EMBER_LOGGER_ZIGBEE_JOIN_NETWORK_LENGTH 12

The length of the Join Network event data.

#define
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_REJOIN_LENGTH 5

The length of the Trust Center Rejoin event data.

#define
EMBER_LOGGER_ZIGBEE_SECURE_REJOIN_LENGTH 5

The length of the Secure Rejoin event data.

#define
EMBER_LOGGER_ZIGBEE_LEAVE_WITHOUT_REJOIN_LENGTH 3

The length of the Leave Without Rejoin event data.

#define
EMBER_LOGGER_ZIGBEE_LEAVE_WITH_REJOIN_LENGTH 3

The length of the Leave With Rejoin event data.

#define
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_LINK_KEY_CHANGE_LENGTH 0

The length of the Trust Center Link Key Change event data.

#define
EMBER_LOGGER_ZIGBEE_NETWORK_KEY_SEQUENCE_NUMBER_CHANGE_LENGTH 1

The length of the Network Key Sequence Number Change event data.

#define
EMBER_LOGGER_ZIGBEE_RESET_LENGTH 2

The length of the Reset event data.

#define
EMBER_LOGGER_ZIGBEE_CHANNEL_CHANGE_LENGTH 2

The length of the Channel Change event data.

#define
EMBER_LOGGER_ZIGBEE_PARENT_CHANGE_LENGTH 10

The length of the Parent Change event data.

#define
EMBER_LOGGER_ZIGBEE_DUTY_CYCLE_CHANGE_LENGTH 7

The length of the Duty Cycle Change event data.

#define
EMBER_LOGGER_ZIGBEE_CHILD_ADDED_LENGTH 10

The length of the Child Added event data.

#define
EMBER_LOGGER_ZIGBEE_CHILD_REMOVED_LENGTH 10

The length of the Child Removed event data.

#define
EMBER_LOGGER_ZIGBEE_CHILD_TIMED_OUT_LENGTH 10

The length of the Child Timed Out event data.

#define
EMBER_LOGGER_ZIGBEE_STACK_STATUS_LENGTH 1

The length of the Stack Status event data.

#define
EMBER_LOGGER_ZIGBEE_TIME_SYNC_LENGTH 8

The length of the Time Sync event data.

#define
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_JOIN_DECISION_LENGTH 3

The length of the Trust Center Join Decision event data.

Enumeration Documentation#

EmberZigbeeLoggerEventTypes#

EmberZigbeeLoggerEventTypes

A list of identifiers for system events.

Enumerator
EMBER_LOGGER_ZIGBEE_BOOT_EVENT_ID
EMBER_LOGGER_ZIGBEE_JOIN_NETWORK_ID
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_REJOIN_ID
EMBER_LOGGER_ZIGBEE_SECURE_REJOIN_ID
EMBER_LOGGER_ZIGBEE_LEAVE_WITHOUT_REJOIN_ID
EMBER_LOGGER_ZIGBEE_LEAVE_WITH_REJOIN_ID
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_LINK_KEY_CHANGE_ID
EMBER_LOGGER_ZIGBEE_NETWORK_KEY_SEQUENCE_NUMBER_CHANGE_ID
EMBER_LOGGER_ZIGBEE_RESET_ID
EMBER_LOGGER_ZIGBEE_CHANNEL_CHANGE_ID
EMBER_LOGGER_ZIGBEE_PARENT_CHANGE_ID
EMBER_LOGGER_ZIGBEE_DUTY_CYCLE_CHANGE_ID
EMBER_LOGGER_ZIGBEE_CHILD_ADDED_ID
EMBER_LOGGER_ZIGBEE_CHILD_REMOVED_ID
EMBER_LOGGER_ZIGBEE_CHILD_TIMED_OUT_ID
EMBER_LOGGER_ZIGBEE_STACK_STATUS_ID
EMBER_LOGGER_ZIGBEE_TIME_SYNC_ID
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_JOIN_DECISION_ID
EMBER_LOGGER_ZIGBEE_NULL_ID

EmberZigbeeLoggerFacilityTypes#

EmberZigbeeLoggerFacilityTypes

A list of facilities for system events, identifying which layer they occurred in.

Enumerator
EMBER_LOGGER_ZIGBEE_FACILITY_BASE
EMBER_LOGGER_ZIGBEE_FACILITY_MAC
EMBER_LOGGER_ZIGBEE_FACILITY_NETWORK
EMBER_LOGGER_ZIGBEE_FACILITY_APS
EMBER_LOGGER_ZIGBEE_FACILITY_SECURITY
EMBER_LOGGER_ZIGBEE_FACILITY_ZDO
EMBER_LOGGER_ZIGBEE_FACILITY_ZCL
EMBER_LOGGER_ZIGBEE_FACILITY_BDB
EMBER_LOGGER_ZIGBEE_FACILITY_SMART_ENERGY

Function Documentation#

emberAfPluginZigBeeEventLoggerAddBootEvent#

void emberAfPluginZigBeeEventLoggerAddBootEvent (uint32_t bootCount, uint16_t resetType)

Record an event indicating that the device has booted.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/AbootCount

The number of times the device has booted.

uint16_tN/AresetType

A reset cause. See micro.h and reset-def.h.

Note

  • This API only works on SoC. It does not work on host or NCP.


emberAfPluginZigBeeEventLoggerAddJoinNetwork#

void emberAfPluginZigBeeEventLoggerAddJoinNetwork (EmberPanId panId, uint8_t channelNumber, uint8_t page, uint8_t * extendedPanId)

Record an event indicating that a network was successfully joined.

Parameters
TypeDirectionArgument NameDescription
EmberPanIdN/ApanId

The PAN ID of the network.

uint8_tN/AchannelNumber

The channel of the network.

uint8_tN/Apage

The page of the network joined.

uint8_t *N/AextendedPanId

The extended PAN ID of the network.


emberAfPluginZigBeeEventLoggerAddTrustCenterRejoin#

void emberAfPluginZigBeeEventLoggerAddTrustCenterRejoin (uint32_t channelMask, EmberRejoinReason reason)

Record an event indicating that a trust center rejoin was attempted.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/AchannelMask

The channel mask used when searching for the network.

EmberRejoinReasonN/Areason

An EmberRejoinReason enumeration, indicating why the rejoin was initiated.

Note

  • This event only indicates that a rejoin was attempted, not that it was successful. A Join Network event, following this event, indicates success.


emberAfPluginZigBeeEventLoggerAddSecureRejoin#

void emberAfPluginZigBeeEventLoggerAddSecureRejoin (uint32_t channelMask, EmberRejoinReason reason)

Record an event indicating that a secure rejoin was attempted.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/AchannelMask

The channel mask used when searching for the network.

EmberRejoinReasonN/Areason

An EmberRejoinReason enumeration, indicating why the rejoin was initiated.

Note

  • This event only indicates that a rejoin was attempted, not that it was successful. A Join Network event, following this event, indicates success.


emberAfPluginZigBeeEventLoggerAddLeaveWithoutRejoin#

void emberAfPluginZigBeeEventLoggerAddLeaveWithoutRejoin (EmberNodeId sourceNode, EmberLeaveReason reason)

Record an event indicating that a device has left-without-rejoin.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AsourceNode

The node ID of the device leaving.

EmberLeaveReasonN/Areason

An EmberLeaveReason enumeration, indicating why the device left.


emberAfPluginZigBeeEventLoggerAddLeaveWithRejoin#

void emberAfPluginZigBeeEventLoggerAddLeaveWithRejoin (EmberNodeId sourceNode, EmberLeaveReason reason)

Record an event indicating that a device has left-with-rejoin.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AsourceNode

The node ID of the device leaving-and-rejoining.

EmberLeaveReasonN/Areason

An EmberLeaveReason enumeration, indicating why the device left.


emberAfPluginZigBeeEventLoggerAddTrustCenterLinkKeyChange#

void emberAfPluginZigBeeEventLoggerAddTrustCenterLinkKeyChange (void )

Record an event indicating that an attempt was made to update the trust center link key.

Parameters
TypeDirectionArgument NameDescription
voidN/A

emberAfPluginZigBeeEventLoggerAddNetworkKeySequenceChange#

void emberAfPluginZigBeeEventLoggerAddNetworkKeySequenceChange (uint8_t sequence)

Record an event indicating that the network key sequence number has changed.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Asequence

The new network key sequence number.


emberAfPluginZigBeeEventLoggerAddReset#

void emberAfPluginZigBeeEventLoggerAddReset (uint8_t resetCode, uint8_t extendedReason)

Record an event indicating that the local device has reset.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/AresetCode

The reset code. See reset-def.h.

uint8_tN/AextendedReason

The extended reset reason. See reset-def.h.


emberAfPluginZigBeeEventLoggerAddChannelChange#

void emberAfPluginZigBeeEventLoggerAddChannelChange (uint8_t page, uint8_t channel)

Record an event indicating that the network's channel has changed.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Apage

The new page number.

uint8_tN/Achannel

The new channel number.


emberAfPluginZigBeeEventLoggerAddParentChange#

void emberAfPluginZigBeeEventLoggerAddParentChange (EmberNodeId parentNodeId, EmberEUI64 parentEui64)

Record an event indicating that the local device's parent has changed.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AparentNodeId

The new parent's short address.

EmberEUI64N/AparentEui64

The new parent's long address.


emberAfPluginZigBeeEventLoggerAddDutyCycleChange#

void emberAfPluginZigBeeEventLoggerAddDutyCycleChange (EmberDutyCycleState state, EmberDutyCycleHectoPct limitThreshold, EmberDutyCycleHectoPct criticalThreshold, EmberDutyCycleHectoPct suspendedLimit)

Record an event indicating that the duty cycle has changed.

Parameters
TypeDirectionArgument NameDescription
EmberDutyCycleStateN/Astate

An EmberDutyCycleState state.

EmberDutyCycleHectoPctN/AlimitThreshold

An EmberDutyCycleHectoPct limit.

EmberDutyCycleHectoPctN/AcriticalThreshold

An EmberDutyCycleHectoPct critical threshold.

EmberDutyCycleHectoPctN/AsuspendedLimit

An EmberDutyCycleHectoPct suspend limit.


emberAfPluginZigBeeEventLoggerAddChildAdded#

void emberAfPluginZigBeeEventLoggerAddChildAdded (EmberNodeId childNodeId, EmberEUI64 childEui64)

Record an event indicating that a child device has joined the local device.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AchildNodeId

The child's short address.

EmberEUI64N/AchildEui64

The child's long address.


emberAfPluginZigBeeEventLoggerAddChildRemoved#

void emberAfPluginZigBeeEventLoggerAddChildRemoved (EmberNodeId childNodeId, EmberEUI64 childEui64)

Record an event indicating that a child device has been removed from the local device.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AchildNodeId

The child's short address.

EmberEUI64N/AchildEui64

The child's long address.


emberAfPluginZigBeeEventLoggerAddChildTimedOut#

void emberAfPluginZigBeeEventLoggerAddChildTimedOut (EmberNodeId childNodeId, EmberEUI64 childEui64)

Record an event indicating that a child device has been timed out by the local device.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AchildNodeId

The child's short address.

EmberEUI64N/AchildEui64

The child's long address.


emberAfPluginZigBeeEventLoggerAddStackStatus#

void emberAfPluginZigBeeEventLoggerAddStackStatus (EmberStatus status)

Record an event indicating that the stack status has changed.

Parameters
TypeDirectionArgument NameDescription
EmberStatusN/Astatus

An EmberStatus value indicating the change.


emberAfPluginZigBeeEventLoggerAddTimeSync#

void emberAfPluginZigBeeEventLoggerAddTimeSync (uint32_t utcTime, uint32_t secondsSinceBoot)

Record an event indicating that the clock time has been synchronized.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/AutcTime

The updated UTC time.

uint32_tN/AsecondsSinceBoot

The number of seconds that have elapsed since boot.


emberAfPluginZigBeeEventLoggerAddTrustCenterJoinDecision#

void emberAfPluginZigBeeEventLoggerAddTrustCenterJoinDecision (EmberNodeId nodeId, uint8_t decision)

Record an event indicating that a device has attempted to join or rejoin the network.

Parameters
TypeDirectionArgument NameDescription
EmberNodeIdN/AnodeId

The short address of the device attempting to join or rejoin.

uint8_tN/Adecision

The join or rejoin decision taken by the local device.

Note

  • This event is only recorded on a trust center device.