Public Attribute Documentation#

stackProfile#

uint8_t EmberNetworkInfo::stackProfile

Definition at line 3854 of file stack/include/ember-types.h

nodeType#

uint8_t EmberNetworkInfo::nodeType

Definition at line 3855 of file stack/include/ember-types.h

zigbeeState#

uint8_t EmberNetworkInfo::zigbeeState

Definition at line 3856 of file stack/include/ember-types.h

dynamicCapabilities#

uint8_t EmberNetworkInfo::dynamicCapabilities

Definition at line 3857 of file stack/include/ember-types.h

zigbeeNetworkSecurityLevel#

uint8_t EmberNetworkInfo::zigbeeNetworkSecurityLevel

Definition at line 3859 of file stack/include/ember-types.h

securityStateBitmask#

uint32_t EmberNetworkInfo::securityStateBitmask

Definition at line 3860 of file stack/include/ember-types.h

zigbeeSequenceNumber#

uint8_t EmberNetworkInfo::zigbeeSequenceNumber

Definition at line 3861 of file stack/include/ember-types.h

apsSequenceNumber#

uint8_t EmberNetworkInfo::apsSequenceNumber

Definition at line 3862 of file stack/include/ember-types.h

securityKeySequenceNumber#

uint8_t EmberNetworkInfo::securityKeySequenceNumber

Definition at line 3865 of file stack/include/ember-types.h

nextNwkFrameCounter#

uint32_t EmberNetworkInfo::nextNwkFrameCounter

Definition at line 3866 of file stack/include/ember-types.h

incomingTcLinkKeyFrameCounter#

uint32_t EmberNetworkInfo::incomingTcLinkKeyFrameCounter

Definition at line 3869 of file stack/include/ember-types.h

neighborTable#

sli_zigbee_neighbor_table_entry_t* EmberNetworkInfo::neighborTable

Definition at line 3872 of file stack/include/ember-types.h

neighborTableSize#

uint8_t EmberNetworkInfo::neighborTableSize

Definition at line 3873 of file stack/include/ember-types.h

neighborCount#

uint8_t EmberNetworkInfo::neighborCount

Definition at line 3874 of file stack/include/ember-types.h

frameCounters#

uint32_t* EmberNetworkInfo::frameCounters

Definition at line 3877 of file stack/include/ember-types.h

ticksSinceLastPoll#

uint32_t EmberNetworkInfo::ticksSinceLastPoll

Definition at line 3881 of file stack/include/ember-types.h

msSinceLastPoll#

uint32_t EmberNetworkInfo::msSinceLastPoll

Definition at line 3882 of file stack/include/ember-types.h

unicastTxAttempts#

uint16_t EmberNetworkInfo::unicastTxAttempts

Definition at line 3886 of file stack/include/ember-types.h

unicastTxFailures#

uint16_t EmberNetworkInfo::unicastTxFailures

Definition at line 3887 of file stack/include/ember-types.h

parentNwkInformation#

uint16_t EmberNetworkInfo::parentNwkInformation

Definition at line 3888 of file stack/include/ember-types.h

lastChildAgeTimeSeconds#

uint16_t EmberNetworkInfo::lastChildAgeTimeSeconds

Definition at line 3895 of file stack/include/ember-types.h

lastChildAgeTimeMs#

uint32_t EmberNetworkInfo::lastChildAgeTimeMs

Definition at line 3896 of file stack/include/ember-types.h

panInfoData#

sli_zigbee_pan_info_t* EmberNetworkInfo::panInfoData

Definition at line 3900 of file stack/include/ember-types.h