Return-code definitions for EmberZNet stack API functions.

See Status Codes for documentation.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

/***************************************************************************/
#ifndef SILABS_ERROR_DEF_H
#define SILABS_ERROR_DEF_H

#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberStatus
#else
enum
#endif //DOXYGEN_SHOULD_SKIP_THIS
{

  EMBER_SUCCESS = 0x00,

  EMBER_ERR_FATAL = 0x01,

  EMBER_BAD_ARGUMENT = 0x02,

  EMBER_NOT_FOUND = 0x03,

  EMBER_EEPROM_MFG_STACK_VERSION_MISMATCH = 0x04,

  EMBER_EEPROM_MFG_VERSION_MISMATCH = 0x06,

  EMBER_EEPROM_STACK_VERSION_MISMATCH = 0x07,



  EMBER_NO_BUFFERS = 0x18,

  EMBER_PACKET_HANDOFF_DROP_PACKET = 0x19,



  EMBER_SERIAL_INVALID_BAUD_RATE = 0x20,

  EMBER_SERIAL_INVALID_PORT = 0x21,

  EMBER_SERIAL_TX_OVERFLOW = 0x22,

  EMBER_SERIAL_RX_OVERFLOW = 0x23,

  EMBER_SERIAL_RX_FRAME_ERROR = 0x24,

  EMBER_SERIAL_RX_PARITY_ERROR = 0x25,

  EMBER_SERIAL_RX_EMPTY = 0x26,

  EMBER_SERIAL_RX_OVERRUN_ERROR = 0x27,



  EMBER_MAC_TRANSMIT_QUEUE_FULL = 0x39,
// Internal

  EMBER_MAC_UNKNOWN_HEADER_TYPE = 0x3A,

  EMBER_MAC_ACK_HEADER_TYPE = 0x3B,

  EMBER_MAC_SCANNING = 0x3D,

  EMBER_MAC_NO_DATA = 0x31,

  EMBER_MAC_JOINED_NETWORK = 0x32,

  EMBER_MAC_BAD_SCAN_DURATION = 0x33,

  EMBER_MAC_INCORRECT_SCAN_TYPE = 0x34,

  EMBER_MAC_INVALID_CHANNEL_MASK = 0x35,

  EMBER_MAC_COMMAND_TRANSMIT_FAILURE = 0x36,

  EMBER_MAC_NO_ACK_RECEIVED = 0x40,

  EMBER_MAC_RADIO_NETWORK_SWITCH_FAILED = 0x41,

  EMBER_MAC_INDIRECT_TIMEOUT = 0x42,



  EMBER_SIM_EEPROM_ERASE_PAGE_GREEN = 0x43,

  EMBER_SIM_EEPROM_ERASE_PAGE_RED = 0x44,

  EMBER_SIM_EEPROM_FULL = 0x45,

//  Errors 46 and 47 are now defined below in the
//    flash error block  (was attempting to prevent renumbering).

  EMBER_SIM_EEPROM_INIT_1_FAILED = 0x48,

  EMBER_SIM_EEPROM_INIT_2_FAILED = 0x49,

  EMBER_SIM_EEPROM_INIT_3_FAILED = 0x4A,

  EMBER_SIM_EEPROM_REPAIRING = 0x4D,



  EMBER_ERR_FLASH_WRITE_INHIBITED = 0x46,

  EMBER_ERR_FLASH_VERIFY_FAILED = 0x47,

  EMBER_ERR_FLASH_PROG_FAIL = 0x4B,

  EMBER_ERR_FLASH_ERASE_FAIL = 0x4C,



  EMBER_ERR_BOOTLOADER_TRAP_TABLE_BAD = 0x58,

  EMBER_ERR_BOOTLOADER_TRAP_UNKNOWN = 0x59,

  EMBER_ERR_BOOTLOADER_NO_IMAGE = 0x05A,



  EMBER_DELIVERY_FAILED = 0x66,

  EMBER_BINDING_INDEX_OUT_OF_RANGE = 0x69,

  EMBER_ADDRESS_TABLE_INDEX_OUT_OF_RANGE = 0x6A,

  EMBER_INVALID_BINDING_INDEX = 0x6C,

  EMBER_INVALID_CALL = 0x70,

  EMBER_COST_NOT_KNOWN = 0x71,

  EMBER_MAX_MESSAGE_LIMIT_REACHED = 0x72,

  EMBER_MESSAGE_TOO_LONG = 0x74,

  EMBER_BINDING_IS_ACTIVE = 0x75,

  EMBER_ADDRESS_TABLE_ENTRY_IS_ACTIVE = 0x76,

  EMBER_TRANSMISSION_SUSPENDED = 0x77,

//


  EMBER_MATCH = 0x78,
  EMBER_DROP_FRAME = 0x79,
  EMBER_PASS_UNPROCESSED = 0x7A,
  EMBER_TX_THEN_DROP = 0x7B,
  EMBER_NO_SECURITY = 0x7C,
  EMBER_COUNTER_FAILURE = 0x7D,
  EMBER_AUTH_FAILURE = 0x7E,
  EMBER_UNPROCESSED = 0x7F,

//


  EMBER_ADC_CONVERSION_DONE = 0x80,

  EMBER_ADC_CONVERSION_BUSY = 0x81,

  EMBER_ADC_CONVERSION_DEFERRED = 0x82,

  EMBER_ADC_NO_CONVERSION_PENDING = 0x84,

  EMBER_SLEEP_INTERRUPTED = 0x85,



  EMBER_PHY_TX_SCHED_FAIL = 0x87,

  EMBER_PHY_TX_UNDERFLOW = 0x88,

  EMBER_PHY_TX_INCOMPLETE = 0x89,

  EMBER_PHY_INVALID_CHANNEL = 0x8A,

  EMBER_PHY_INVALID_POWER = 0x8B,

  EMBER_PHY_TX_BUSY = 0x8C,

  EMBER_PHY_TX_CCA_FAIL = 0x8D,

  EMBER_PHY_TX_BLOCKED = 0x8E,

  EMBER_PHY_ACK_RECEIVED = 0x8F,



  EMBER_NETWORK_UP = 0x90,

  EMBER_NETWORK_DOWN = 0x91,

  EMBER_JOIN_FAILED = 0x94,

  EMBER_MOVE_FAILED = 0x96,

  EMBER_CANNOT_JOIN_AS_ROUTER = 0x98,

  EMBER_NODE_ID_CHANGED = 0x99,

  EMBER_PAN_ID_CHANGED = 0x9A,

  EMBER_CHANNEL_CHANGED = 0x9B,

  EMBER_NETWORK_OPENED = 0x9C,

  EMBER_NETWORK_CLOSED = 0x9D,

  EMBER_NO_BEACONS = 0xAB,

  EMBER_RECEIVED_KEY_IN_THE_CLEAR = 0xAC,

  EMBER_NO_NETWORK_KEY_RECEIVED = 0xAD,

  EMBER_NO_LINK_KEY_RECEIVED = 0xAE,

  EMBER_PRECONFIGURED_KEY_REQUIRED = 0xAF,


  EMBER_KEY_INVALID = 0xB2,

  EMBER_INVALID_SECURITY_LEVEL = 0x95,

  EMBER_IEEE_ADDRESS_DISCOVERY_IN_PROGRESS = 0xBE,
  EMBER_APS_ENCRYPTION_ERROR = 0xA6,

  EMBER_SECURITY_STATE_NOT_SET = 0xA8,

  EMBER_KEY_TABLE_INVALID_ADDRESS = 0xB3,

  EMBER_SECURITY_CONFIGURATION_INVALID = 0xB7,

  EMBER_TOO_SOON_FOR_SWITCH_KEY = 0xB8,

  EMBER_SIGNATURE_VERIFY_FAILURE = 0xB9,

  EMBER_KEY_NOT_AUTHORIZED = 0xBB,

  EMBER_SECURITY_DATA_INVALID = 0xBD,



  EMBER_NOT_JOINED = 0x93,

  EMBER_NETWORK_BUSY = 0xA1,

  EMBER_INVALID_ENDPOINT = 0xA3,

  EMBER_BINDING_HAS_CHANGED = 0xA4,

  EMBER_INSUFFICIENT_RANDOM_DATA = 0xA5,

  EMBER_SOURCE_ROUTE_FAILURE = 0xA9,

  EMBER_MANY_TO_ONE_ROUTE_FAILURE = 0xAA,



  EMBER_STACK_AND_HARDWARE_MISMATCH = 0xB0,

  EMBER_INDEX_OUT_OF_RANGE = 0xB1,

  EMBER_TABLE_FULL = 0xB4,

  EMBER_TABLE_ENTRY_ERASED = 0xB6,

  EMBER_LIBRARY_NOT_PRESENT = 0xB5,

  EMBER_OPERATION_IN_PROGRESS = 0xBA,

  EMBER_TRUST_CENTER_EUI_HAS_CHANGED = 0xBC,

  EMBER_TRUST_CENTER_SWAPPED_OUT_EUI_HAS_CHANGED = EMBER_TRUST_CENTER_EUI_HAS_CHANGED,

  EMBER_TRUST_CENTER_SWAPPED_OUT_EUI_HAS_NOT_CHANGED = 0xBF,



  EMBER_NVM3_TOKEN_NO_VALID_PAGES = 0xC0,

  EMBER_NVM3_ERR_OPENED_WITH_OTHER_PARAMETERS = 0xC1,

  EMBER_NVM3_ERR_ALIGNMENT_INVALID = 0xC2,

  EMBER_NVM3_ERR_SIZE_TOO_SMALL = 0xC3,

  EMBER_NVM3_ERR_PAGE_SIZE_NOT_SUPPORTED = 0xC4,

  EMBER_NVM3_ERR_TOKEN_INIT = 0xC5,

  EMBER_NVM3_ERR_UPGRADE = 0xC6,

  EMBER_NVM3_ERR_UNKNOWN = 0xC7,



  EMBER_APPLICATION_ERROR_0 = 0xF0,
  EMBER_APPLICATION_ERROR_1 = 0xF1,
  EMBER_APPLICATION_ERROR_2 = 0xF2,
  EMBER_APPLICATION_ERROR_3 = 0xF3,
  EMBER_APPLICATION_ERROR_4 = 0xF4,
  EMBER_APPLICATION_ERROR_5 = 0xF5,
  EMBER_APPLICATION_ERROR_6 = 0xF6,
  EMBER_APPLICATION_ERROR_7 = 0xF7,
  EMBER_APPLICATION_ERROR_8 = 0xF8,
  EMBER_APPLICATION_ERROR_9 = 0xF9,
  EMBER_APPLICATION_ERROR_10 = 0xFA,
  EMBER_APPLICATION_ERROR_11 = 0xFB,
  EMBER_APPLICATION_ERROR_12 = 0xFC,
  EMBER_APPLICATION_ERROR_13 = 0xFD,
  EMBER_APPLICATION_ERROR_14 = 0xFE,
  EMBER_APPLICATION_ERROR_15 = 0xFF,
};


#endif // SILABS_ERROR_DEF_H

Enumerations#

enum
EMBER_SUCCESS = 0x00
EMBER_ERR_FATAL = 0x01
EMBER_BAD_ARGUMENT = 0x02
EMBER_NOT_FOUND = 0x03
EMBER_EEPROM_MFG_STACK_VERSION_MISMATCH = 0x04
EMBER_EEPROM_MFG_VERSION_MISMATCH = 0x06
EMBER_EEPROM_STACK_VERSION_MISMATCH = 0x07
EMBER_NO_BUFFERS = 0x18
EMBER_PACKET_HANDOFF_DROP_PACKET = 0x19
EMBER_SERIAL_INVALID_BAUD_RATE = 0x20
EMBER_SERIAL_INVALID_PORT = 0x21
EMBER_SERIAL_TX_OVERFLOW = 0x22
EMBER_SERIAL_RX_OVERFLOW = 0x23
EMBER_SERIAL_RX_FRAME_ERROR = 0x24
EMBER_SERIAL_RX_PARITY_ERROR = 0x25
EMBER_SERIAL_RX_EMPTY = 0x26
EMBER_SERIAL_RX_OVERRUN_ERROR = 0x27
EMBER_MAC_TRANSMIT_QUEUE_FULL = 0x39
EMBER_MAC_UNKNOWN_HEADER_TYPE = 0x3A
EMBER_MAC_ACK_HEADER_TYPE = 0x3B
EMBER_MAC_SCANNING = 0x3D
EMBER_MAC_NO_DATA = 0x31
EMBER_MAC_JOINED_NETWORK = 0x32
EMBER_MAC_BAD_SCAN_DURATION = 0x33
EMBER_MAC_INCORRECT_SCAN_TYPE = 0x34
EMBER_MAC_INVALID_CHANNEL_MASK = 0x35
EMBER_MAC_COMMAND_TRANSMIT_FAILURE = 0x36
EMBER_MAC_NO_ACK_RECEIVED = 0x40
EMBER_MAC_RADIO_NETWORK_SWITCH_FAILED = 0x41
EMBER_MAC_INDIRECT_TIMEOUT = 0x42
EMBER_SIM_EEPROM_ERASE_PAGE_GREEN = 0x43
EMBER_SIM_EEPROM_ERASE_PAGE_RED = 0x44
EMBER_SIM_EEPROM_FULL = 0x45
EMBER_SIM_EEPROM_INIT_1_FAILED = 0x48
EMBER_SIM_EEPROM_INIT_2_FAILED = 0x49
EMBER_SIM_EEPROM_INIT_3_FAILED = 0x4A
EMBER_SIM_EEPROM_REPAIRING = 0x4D
EMBER_ERR_FLASH_WRITE_INHIBITED = 0x46
EMBER_ERR_FLASH_VERIFY_FAILED = 0x47
EMBER_ERR_FLASH_PROG_FAIL = 0x4B
EMBER_ERR_FLASH_ERASE_FAIL = 0x4C
EMBER_ERR_BOOTLOADER_TRAP_TABLE_BAD = 0x58
EMBER_ERR_BOOTLOADER_TRAP_UNKNOWN = 0x59
EMBER_ERR_BOOTLOADER_NO_IMAGE = 0x05A
EMBER_DELIVERY_FAILED = 0x66
EMBER_BINDING_INDEX_OUT_OF_RANGE = 0x69
EMBER_ADDRESS_TABLE_INDEX_OUT_OF_RANGE = 0x6A
EMBER_INVALID_BINDING_INDEX = 0x6C
EMBER_INVALID_CALL = 0x70
EMBER_COST_NOT_KNOWN = 0x71
EMBER_MAX_MESSAGE_LIMIT_REACHED = 0x72
EMBER_MESSAGE_TOO_LONG = 0x74
EMBER_BINDING_IS_ACTIVE = 0x75
EMBER_ADDRESS_TABLE_ENTRY_IS_ACTIVE = 0x76
EMBER_TRANSMISSION_SUSPENDED = 0x77
EMBER_MATCH = 0x78
EMBER_DROP_FRAME = 0x79
EMBER_PASS_UNPROCESSED = 0x7A
EMBER_TX_THEN_DROP = 0x7B
EMBER_NO_SECURITY = 0x7C
EMBER_COUNTER_FAILURE = 0x7D
EMBER_AUTH_FAILURE = 0x7E
EMBER_UNPROCESSED = 0x7F
EMBER_ADC_CONVERSION_DONE = 0x80
EMBER_ADC_CONVERSION_BUSY = 0x81
EMBER_ADC_CONVERSION_DEFERRED = 0x82
EMBER_ADC_NO_CONVERSION_PENDING = 0x84
EMBER_SLEEP_INTERRUPTED = 0x85
EMBER_PHY_TX_SCHED_FAIL = 0x87
EMBER_PHY_TX_UNDERFLOW = 0x88
EMBER_PHY_TX_INCOMPLETE = 0x89
EMBER_PHY_INVALID_CHANNEL = 0x8A
EMBER_PHY_INVALID_POWER = 0x8B
EMBER_PHY_TX_BUSY = 0x8C
EMBER_PHY_TX_CCA_FAIL = 0x8D
EMBER_PHY_TX_BLOCKED = 0x8E
EMBER_PHY_ACK_RECEIVED = 0x8F
EMBER_NETWORK_UP = 0x90
EMBER_NETWORK_DOWN = 0x91
EMBER_JOIN_FAILED = 0x94
EMBER_MOVE_FAILED = 0x96
EMBER_CANNOT_JOIN_AS_ROUTER = 0x98
EMBER_NODE_ID_CHANGED = 0x99
EMBER_PAN_ID_CHANGED = 0x9A
EMBER_CHANNEL_CHANGED = 0x9B
EMBER_NETWORK_OPENED = 0x9C
EMBER_NETWORK_CLOSED = 0x9D
EMBER_NO_BEACONS = 0xAB
EMBER_RECEIVED_KEY_IN_THE_CLEAR = 0xAC
EMBER_NO_NETWORK_KEY_RECEIVED = 0xAD
EMBER_NO_LINK_KEY_RECEIVED = 0xAE
EMBER_PRECONFIGURED_KEY_REQUIRED = 0xAF
EMBER_KEY_INVALID = 0xB2
EMBER_INVALID_SECURITY_LEVEL = 0x95
EMBER_IEEE_ADDRESS_DISCOVERY_IN_PROGRESS = 0xBE
EMBER_APS_ENCRYPTION_ERROR = 0xA6
EMBER_SECURITY_STATE_NOT_SET = 0xA8
EMBER_KEY_TABLE_INVALID_ADDRESS = 0xB3
EMBER_SECURITY_CONFIGURATION_INVALID = 0xB7
EMBER_TOO_SOON_FOR_SWITCH_KEY = 0xB8
EMBER_SIGNATURE_VERIFY_FAILURE = 0xB9
EMBER_KEY_NOT_AUTHORIZED = 0xBB
EMBER_SECURITY_DATA_INVALID = 0xBD
EMBER_NOT_JOINED = 0x93
EMBER_NETWORK_BUSY = 0xA1
EMBER_INVALID_ENDPOINT = 0xA3
EMBER_BINDING_HAS_CHANGED = 0xA4
EMBER_INSUFFICIENT_RANDOM_DATA = 0xA5
EMBER_SOURCE_ROUTE_FAILURE = 0xA9
EMBER_MANY_TO_ONE_ROUTE_FAILURE = 0xAA
EMBER_STACK_AND_HARDWARE_MISMATCH = 0xB0
EMBER_INDEX_OUT_OF_RANGE = 0xB1
EMBER_TABLE_FULL = 0xB4
EMBER_TABLE_ENTRY_ERASED = 0xB6
EMBER_LIBRARY_NOT_PRESENT = 0xB5
EMBER_OPERATION_IN_PROGRESS = 0xBA
EMBER_TRUST_CENTER_EUI_HAS_CHANGED = 0xBC
EMBER_TRUST_CENTER_SWAPPED_OUT_EUI_HAS_CHANGED = EMBER_TRUST_CENTER_EUI_HAS_CHANGED
EMBER_TRUST_CENTER_SWAPPED_OUT_EUI_HAS_NOT_CHANGED = 0xBF
EMBER_NVM3_TOKEN_NO_VALID_PAGES = 0xC0
EMBER_NVM3_ERR_OPENED_WITH_OTHER_PARAMETERS = 0xC1
EMBER_NVM3_ERR_ALIGNMENT_INVALID = 0xC2
EMBER_NVM3_ERR_SIZE_TOO_SMALL = 0xC3
EMBER_NVM3_ERR_PAGE_SIZE_NOT_SUPPORTED = 0xC4
EMBER_NVM3_ERR_TOKEN_INIT = 0xC5
EMBER_NVM3_ERR_UPGRADE = 0xC6
EMBER_NVM3_ERR_UNKNOWN = 0xC7
EMBER_APPLICATION_ERROR_0 = 0xF0
EMBER_APPLICATION_ERROR_1 = 0xF1
EMBER_APPLICATION_ERROR_2 = 0xF2
EMBER_APPLICATION_ERROR_3 = 0xF3
EMBER_APPLICATION_ERROR_4 = 0xF4
EMBER_APPLICATION_ERROR_5 = 0xF5
EMBER_APPLICATION_ERROR_6 = 0xF6
EMBER_APPLICATION_ERROR_7 = 0xF7
EMBER_APPLICATION_ERROR_8 = 0xF8
EMBER_APPLICATION_ERROR_9 = 0xF9
EMBER_APPLICATION_ERROR_10 = 0xFA
EMBER_APPLICATION_ERROR_11 = 0xFB
EMBER_APPLICATION_ERROR_12 = 0xFC
EMBER_APPLICATION_ERROR_13 = 0xFD
EMBER_APPLICATION_ERROR_14 = 0xFE
EMBER_APPLICATION_ERROR_15 = 0xFF
}

Enumeration Documentation#

EmberStatus#

EmberStatus
Enumerator
EMBER_SUCCESS

The generic "no error" message.

EMBER_ERR_FATAL

The generic "fatal error" message.

EMBER_BAD_ARGUMENT

An invalid value was passed as an argument to a function.

EMBER_NOT_FOUND

The requested information was not found.

EMBER_EEPROM_MFG_STACK_VERSION_MISMATCH

The manufacturing and stack token format in non-volatile memory is different than what the stack expects (returned at initialization).

EMBER_EEPROM_MFG_VERSION_MISMATCH

The manufacturing token format in non-volatile memory is different than what the stack expects (returned at initialization).

EMBER_EEPROM_STACK_VERSION_MISMATCH

The stack token format in non-volatile memory is different than what the stack expects (returned at initialization).

EMBER_NO_BUFFERS

There are no more buffers.

EMBER_PACKET_HANDOFF_DROP_PACKET

Packet is dropped by packet-handoff callbacks.

EMBER_SERIAL_INVALID_BAUD_RATE

Specifies an invalid baud rate.

EMBER_SERIAL_INVALID_PORT

Specifies an invalid serial port.

EMBER_SERIAL_TX_OVERFLOW

Tried to send too much data.

EMBER_SERIAL_RX_OVERFLOW

There wasn't enough space to store a received character and the character was dropped.

EMBER_SERIAL_RX_FRAME_ERROR

Detected a UART framing error.

EMBER_SERIAL_RX_PARITY_ERROR

Detected a UART parity error.

EMBER_SERIAL_RX_EMPTY

There is no received data to process.

EMBER_SERIAL_RX_OVERRUN_ERROR

The receive interrupt was not handled in time and a character was dropped.

EMBER_MAC_TRANSMIT_QUEUE_FULL

The MAC transmit queue is full.

EMBER_MAC_UNKNOWN_HEADER_TYPE

MAC header FCF error on receive.

EMBER_MAC_ACK_HEADER_TYPE

MAC ACK header received.

EMBER_MAC_SCANNING

The MAC can't complete this task because it is scanning.

EMBER_MAC_NO_DATA

No pending data exists for a data poll.

EMBER_MAC_JOINED_NETWORK

Attempts to scan when joined to a network.

EMBER_MAC_BAD_SCAN_DURATION

Scan duration must be 0 to 14 inclusive. Tried to scan with an incorrect duration value.

EMBER_MAC_INCORRECT_SCAN_TYPE

emberStartScan was called with an incorrect scan type.

EMBER_MAC_INVALID_CHANNEL_MASK

emberStartScan was called with an invalid channel mask.

EMBER_MAC_COMMAND_TRANSMIT_FAILURE

Failed to scan the current channel because the relevant MAC command could not be transmitted.

EMBER_MAC_NO_ACK_RECEIVED

An ACK was expected following the transmission but the MAC level ACK was never received.

EMBER_MAC_RADIO_NETWORK_SWITCH_FAILED

MAC failed to transmit a message because it could not successfully perform a radio network switch.

EMBER_MAC_INDIRECT_TIMEOUT

An indirect data message timed out before a poll requested it.

EMBER_SIM_EEPROM_ERASE_PAGE_GREEN

The Simulated EEPROM is telling the application that at least one flash page to be erased. The GREEN status means the current page has not filled above the ::ERASE_CRITICAL_THRESHOLD.

EMBER_SIM_EEPROM_ERASE_PAGE_RED

The Simulated EEPROM is telling the application that at least one flash page must be erased. The RED status means the current page has filled above the ::ERASE_CRITICAL_THRESHOLD.

EMBER_SIM_EEPROM_FULL

The Simulated EEPROM has run out of room to write new data and the data trying to be set has been lost. This error code is the result of ignoring the ::SIM_EEPROM_ERASE_PAGE_RED error code.

EMBER_SIM_EEPROM_INIT_1_FAILED

Attempt 1 to initialize the Simulated EEPROM has failed.

EMBER_SIM_EEPROM_INIT_2_FAILED

Attempt 2 to initialize the Simulated EEPROM has failed.

EMBER_SIM_EEPROM_INIT_3_FAILED

Attempt 3 to initialize the Simulated EEPROM has failed.

EMBER_SIM_EEPROM_REPAIRING

The Simulated EEPROM is repairing itself.

EMBER_ERR_FLASH_WRITE_INHIBITED

A fatal error has occurred while trying to write data to the Flash. The target memory attempting to be programmed is already programmed. The flash write routines were asked to flip a bit from a 0 to 1, which is physically impossible and the write was therefore inhibited. The data in the Flash cannot be trusted after this error.

EMBER_ERR_FLASH_VERIFY_FAILED

A fatal error has occurred while trying to write data to the Flash and the write verification has failed. Data in the Flash cannot be trusted after this error and it is possible this error is the result of exceeding the life cycles of the Flash.

EMBER_ERR_FLASH_PROG_FAIL

@description A fatal error has occurred while trying to write data to the Flash possibly due to write protection or an invalid address. Data in the Flash cannot be trusted after this error and it is possible this error is the result of exceeding the life cycles of the Flash.

EMBER_ERR_FLASH_ERASE_FAIL

@description A fatal error has occurred while trying to erase the Flash possibly due to write protection. Data in the Flash cannot be trusted after this error and it is possible this error is the result of exceeding the life cycles of the Flash.

EMBER_ERR_BOOTLOADER_TRAP_TABLE_BAD

The bootloader received an invalid message (failed attempt to go into bootloader).

EMBER_ERR_BOOTLOADER_TRAP_UNKNOWN

The bootloader received an invalid message (failed attempt to go into the bootloader).

EMBER_ERR_BOOTLOADER_NO_IMAGE

The bootloader cannot complete the bootload operation because either an image was not found or the image exceeded memory bounds.

EMBER_DELIVERY_FAILED

The APS layer attempted to send or deliver a message and failed.

EMBER_BINDING_INDEX_OUT_OF_RANGE

This binding index is out of range for the current binding table.

EMBER_ADDRESS_TABLE_INDEX_OUT_OF_RANGE

This address table index is out of range for the current address table.

EMBER_INVALID_BINDING_INDEX

An invalid binding table index was given to a function.

EMBER_INVALID_CALL

The API call is not allowed given the current state of the stack.

EMBER_COST_NOT_KNOWN

The link cost to a node is not known.

EMBER_MAX_MESSAGE_LIMIT_REACHED

The maximum number of in-flight messages = i.e., EMBER_APS_UNICAST_MESSAGE_COUNT, has been reached.

EMBER_MESSAGE_TOO_LONG

The message to be transmitted is too big to fit into a single over-the-air packet.

EMBER_BINDING_IS_ACTIVE

The application is trying to delete or overwrite a binding that is in use.

EMBER_ADDRESS_TABLE_ENTRY_IS_ACTIVE

The application is trying to overwrite an address table entry that is in use.

EMBER_TRANSMISSION_SUSPENDED

An attempt was made to transmit during the suspend period.

EMBER_MATCH

Security match.

EMBER_DROP_FRAME

Drop frame.

EMBER_PASS_UNPROCESSED

Security match.

EMBER_TX_THEN_DROP

Security match.

EMBER_NO_SECURITY

Security match.

EMBER_COUNTER_FAILURE

Security match.

EMBER_AUTH_FAILURE

Security match.

EMBER_UNPROCESSED

Security match.

EMBER_ADC_CONVERSION_DONE

The conversion is complete.

EMBER_ADC_CONVERSION_BUSY

The conversion cannot be done because a request is being processed.

EMBER_ADC_CONVERSION_DEFERRED

The conversion is deferred until the current request has been processed.

EMBER_ADC_NO_CONVERSION_PENDING

No results are pending.

EMBER_SLEEP_INTERRUPTED

Sleeping (for a duration) has been abnormally interrupted and exited prematurely.

EMBER_PHY_TX_SCHED_FAIL

The transmit attempt failed because the radio scheduler could not find a slot to transmit this packet in or a higher priority event interrupted it.

EMBER_PHY_TX_UNDERFLOW

The transmit hardware buffer underflowed.

EMBER_PHY_TX_INCOMPLETE

The transmit hardware did not finish transmitting a packet.

EMBER_PHY_INVALID_CHANNEL

An unsupported channel setting was specified.

EMBER_PHY_INVALID_POWER

An unsupported power setting was specified.

EMBER_PHY_TX_BUSY

The requested operation cannot be completed because the radio is currently busy, either transmitting a packet or performing calibration.

EMBER_PHY_TX_CCA_FAIL

The transmit attempt failed because all CCA attempts indicated that the channel was busy.

EMBER_PHY_TX_BLOCKED

The transmit attempt was blocked from going over the air. Typically this is due to the Radio Hold Off (RHO) or Coexistence plugins as they can prevent transmits based on external signals.

EMBER_PHY_ACK_RECEIVED

The expected ACK was received after the last transmission.

EMBER_NETWORK_UP

The stack software has completed initialization and is ready to send and receive packets over the air.

EMBER_NETWORK_DOWN

The network is not operating.

EMBER_JOIN_FAILED

An attempt to join a network failed.

EMBER_MOVE_FAILED

After moving, a mobile node's attempt to re-establish contact with the network failed.

EMBER_CANNOT_JOIN_AS_ROUTER

An attempt to join as a router failed due to a Zigbee versus Zigbee Pro incompatibility. Zigbee devices joining Zigbee Pro networks (or vice versa) must join as End Devices, not Routers.

EMBER_NODE_ID_CHANGED

The local node ID has changed. The application can get the new node ID by calling emberGetNodeId().

EMBER_PAN_ID_CHANGED

The local PAN ID has changed. The application can get the new PAN ID by calling emberGetPanId().

EMBER_CHANNEL_CHANGED

The channel has changed.

EMBER_NETWORK_OPENED

The network has been opened for joining.

EMBER_NETWORK_CLOSED

The network has been closed for joining.

EMBER_NO_BEACONS

An attempt to join or rejoin the network failed because no router beacons could be heard by the joining node.

EMBER_RECEIVED_KEY_IN_THE_CLEAR

An attempt was made to join a Secured Network using a pre-configured key, but the Trust Center sent back a Network Key in-the-clear when an encrypted Network Key was required. (EMBER_REQUIRE_ENCRYPTED_KEY).

EMBER_NO_NETWORK_KEY_RECEIVED

An attempt was made to join a Secured Network, but the device did not receive a Network Key.

EMBER_NO_LINK_KEY_RECEIVED

After a device joined a Secured Network, a Link Key was requested (EMBER_GET_LINK_KEY_WHEN_JOINING) but no response was ever received.

EMBER_PRECONFIGURED_KEY_REQUIRED

An attempt was made to join a Secured Network without a pre-configured key, but the Trust Center sent encrypted data using a pre-configured key.

EMBER_KEY_INVALID

The passed key data is not valid. A key of all zeros or all F's are reserved values and cannot be used.

EMBER_INVALID_SECURITY_LEVEL

The chosen security level (the value of EMBER_SECURITY_LEVEL) is not supported by the stack.

EMBER_IEEE_ADDRESS_DISCOVERY_IN_PROGRESS

An error occurred when trying to encrypt at the APS Level.

EMBER_APS_ENCRYPTION_ERROR

An error occurred when trying to encrypt at the APS Level.

EMBER_SECURITY_STATE_NOT_SET

There was an attempt to form or join a network with security without calling emberSetInitialSecurityState() first.

EMBER_KEY_TABLE_INVALID_ADDRESS

There was an attempt to set an entry in the key table using an invalid long address. Invalid addresses include:

EMBER_SECURITY_CONFIGURATION_INVALID

There was an attempt to set a security configuration that is not valid given the other security settings.

EMBER_TOO_SOON_FOR_SWITCH_KEY

There was an attempt to broadcast a key switch too quickly after broadcasting the next network key. The Trust Center must wait at least a period equal to the broadcast timeout so that all routers have a chance to receive the broadcast of the new network key.

EMBER_SIGNATURE_VERIFY_FAILURE

The received signature corresponding to the message that was passed to the CBKE Library failed verification and is not valid.

EMBER_KEY_NOT_AUTHORIZED

The message could not be sent because the link key corresponding to the destination is not authorized for use in APS data messages. APS Commands (sent by the stack) are allowed. To use it for encryption of APS data messages it must be authorized using a key agreement protocol (such as CBKE).

EMBER_SECURITY_DATA_INVALID

The security data provided was not valid, or an integrity check failed.

EMBER_NOT_JOINED

The node has not joined a network.

EMBER_NETWORK_BUSY

A message cannot be sent because the network is currently overloaded.

EMBER_INVALID_ENDPOINT

The application tried to send a message using an endpoint that it has not defined.

EMBER_BINDING_HAS_CHANGED

The application tried to use a binding that has been remotely modified and the change has not yet been reported to the application.

EMBER_INSUFFICIENT_RANDOM_DATA

An attempt to generate random bytes failed because of insufficient random data from the radio.

EMBER_SOURCE_ROUTE_FAILURE

A Zigbee route error command frame was received indicating that a source routed message from this node failed en route.

EMBER_MANY_TO_ONE_ROUTE_FAILURE

A Zigbee route error command frame was received indicating that a message sent to this node along a many-to-one route failed en route. The route error frame was delivered by an ad-hoc search for a functioning route.

EMBER_STACK_AND_HARDWARE_MISMATCH

A critical and fatal error indicating that the version of the stack trying to run does not match with the chip it's running on. The software (stack) on the chip must be replaced with software compatible with the chip.

EMBER_INDEX_OUT_OF_RANGE

An index was passed into the function that was larger than the valid range.

EMBER_TABLE_FULL

There are no empty entries left in the table.

EMBER_TABLE_ENTRY_ERASED

The requested table entry has been erased and contains no valid data.

EMBER_LIBRARY_NOT_PRESENT

The requested function cannot be executed because the library that contains the necessary functionality is not present.

EMBER_OPERATION_IN_PROGRESS

The stack accepted the command and is currently processing the request. The results will be returned via an appropriate handler.

EMBER_TRUST_CENTER_EUI_HAS_CHANGED

The EUI of the Trust center has changed due to a successful rejoin. The device may need to perform other authentication to verify the new TC is authorized to take over.

EMBER_TRUST_CENTER_SWAPPED_OUT_EUI_HAS_CHANGED

Trust center swapped out. The EUI has changed.

EMBER_TRUST_CENTER_SWAPPED_OUT_EUI_HAS_NOT_CHANGED

Trust center swapped out. The EUI has not changed.

EMBER_NVM3_TOKEN_NO_VALID_PAGES

NVM3 is telling the application that the initialization was aborted as no valid NVM3 page was found.

EMBER_NVM3_ERR_OPENED_WITH_OTHER_PARAMETERS

NVM3 is telling the application that the initialization was aborted as the NVM3 instance was already opened with other parameters.

EMBER_NVM3_ERR_ALIGNMENT_INVALID

NVM3 is telling the application that the initialization was aborted as the NVM3 instance is not aligned properly in memory.

EMBER_NVM3_ERR_SIZE_TOO_SMALL

NVM3 is telling the application that the initialization was aborted as the size of the NVM3 instance is too small.

EMBER_NVM3_ERR_PAGE_SIZE_NOT_SUPPORTED

NVM3 is telling the application that the initialization was aborted as the NVM3 page size is not supported.

EMBER_NVM3_ERR_TOKEN_INIT

NVM3 is telling the application that there was an error initializing some of the tokens.

EMBER_NVM3_ERR_UPGRADE

NVM3 is telling the application there has been an error when attempting to upgrade SimEE tokens.

EMBER_NVM3_ERR_UNKNOWN

NVM3 is telling the application that there has been an unknown error.

EMBER_APPLICATION_ERROR_0

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_1

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_2

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_3

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_4

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_5

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_6

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_7

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_8

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_9

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_10

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_11

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_12

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_13

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_14

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.

EMBER_APPLICATION_ERROR_15

This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL.


Definition at line 45 of file stack/include/error-def.h