Public Attributes#

EmberNodeId
uint16_t
uint8_t
EmberEUI64

Public Attribute Documentation#

id#

EmberNodeId sli_zigbee_neighbor_table_entry_t::id

Definition at line 3174 of file stack/include/ember-types.h

incoming#

uint16_t sli_zigbee_neighbor_table_entry_t::incoming

Definition at line 3175 of file stack/include/ember-types.h

exchange#

uint8_t sli_zigbee_neighbor_table_entry_t::exchange

Definition at line 3176 of file stack/include/ember-types.h

connectivity#

uint8_t sli_zigbee_neighbor_table_entry_t::connectivity

Definition at line 3179 of file stack/include/ember-types.h

eui64#

EmberEUI64 sli_zigbee_neighbor_table_entry_t::eui64

Definition at line 3187 of file stack/include/ember-types.h

mac_interface_table_index#

uint8_t sli_zigbee_neighbor_table_entry_t::mac_interface_table_index

Definition at line 3188 of file stack/include/ember-types.h

lqi_for_median#

uint8_t sli_zigbee_neighbor_table_entry_t::lqi_for_median[3]

Definition at line 3189 of file stack/include/ember-types.h