Public Attribute Documentation#

stackProfile#

uint8_t sl_zigbee_network_info_t::stackProfile

Definition at line 3215 of file stack/include/sl_zigbee_types.h

nodeType#

uint8_t sl_zigbee_network_info_t::nodeType

Definition at line 3216 of file stack/include/sl_zigbee_types.h

zigbeeState#

uint8_t sl_zigbee_network_info_t::zigbeeState

Definition at line 3217 of file stack/include/sl_zigbee_types.h

dynamicCapabilities#

uint8_t sl_zigbee_network_info_t::dynamicCapabilities

Definition at line 3218 of file stack/include/sl_zigbee_types.h

zigbeeNetworkSecurityLevel#

uint8_t sl_zigbee_network_info_t::zigbeeNetworkSecurityLevel

Definition at line 3220 of file stack/include/sl_zigbee_types.h

securityStateBitmask#

uint32_t sl_zigbee_network_info_t::securityStateBitmask

Definition at line 3221 of file stack/include/sl_zigbee_types.h

zigbeeSequenceNumber#

uint8_t sl_zigbee_network_info_t::zigbeeSequenceNumber

Definition at line 3222 of file stack/include/sl_zigbee_types.h

apsSequenceNumber#

uint8_t sl_zigbee_network_info_t::apsSequenceNumber

Definition at line 3223 of file stack/include/sl_zigbee_types.h

securityKeySequenceNumber#

uint8_t sl_zigbee_network_info_t::securityKeySequenceNumber

Definition at line 3226 of file stack/include/sl_zigbee_types.h

nextNwkFrameCounter#

uint32_t sl_zigbee_network_info_t::nextNwkFrameCounter

Definition at line 3227 of file stack/include/sl_zigbee_types.h

incomingTcLinkKeyFrameCounter#

uint32_t sl_zigbee_network_info_t::incomingTcLinkKeyFrameCounter

Definition at line 3230 of file stack/include/sl_zigbee_types.h

neighborTable#

sl_zigbee_neighbor_table_entry_info_t* sl_zigbee_network_info_t::neighborTable

Definition at line 3233 of file stack/include/sl_zigbee_types.h

neighborTableSize#

uint8_t sl_zigbee_network_info_t::neighborTableSize

Definition at line 3234 of file stack/include/sl_zigbee_types.h

neighborCount#

uint8_t sl_zigbee_network_info_t::neighborCount

Definition at line 3235 of file stack/include/sl_zigbee_types.h

frameCounters#

uint32_t* sl_zigbee_network_info_t::frameCounters

Definition at line 3238 of file stack/include/sl_zigbee_types.h

ticksSinceLastPoll#

uint32_t sl_zigbee_network_info_t::ticksSinceLastPoll

Definition at line 3242 of file stack/include/sl_zigbee_types.h

msSinceLastPoll#

uint32_t sl_zigbee_network_info_t::msSinceLastPoll

Definition at line 3243 of file stack/include/sl_zigbee_types.h

unicastTxAttempts#

uint16_t sl_zigbee_network_info_t::unicastTxAttempts

Definition at line 3247 of file stack/include/sl_zigbee_types.h

unicastTxFailures#

uint16_t sl_zigbee_network_info_t::unicastTxFailures

Definition at line 3248 of file stack/include/sl_zigbee_types.h

parentNwkInformation#

uint16_t sl_zigbee_network_info_t::parentNwkInformation

Definition at line 3249 of file stack/include/sl_zigbee_types.h

lastChildAgeTimeSeconds#

uint16_t sl_zigbee_network_info_t::lastChildAgeTimeSeconds

Definition at line 3256 of file stack/include/sl_zigbee_types.h

lastChildAgeTimeMs#

uint32_t sl_zigbee_network_info_t::lastChildAgeTimeMs

Definition at line 3257 of file stack/include/sl_zigbee_types.h

panInfoData#

sl_zigbee_pan_info_t* sl_zigbee_network_info_t::panInfoData

Definition at line 3261 of file stack/include/sl_zigbee_types.h