Public Attributes#

sl_802154_short_addr_t
uint16_t
uint8_t
sl_802154_long_addr_t

Public Attribute Documentation#

id#

sl_802154_short_addr_t sl_zigbee_neighbor_table_entry_info_t::id

Definition at line 3152 of file stack/include/sl_zigbee_types.h

incoming#

uint16_t sl_zigbee_neighbor_table_entry_info_t::incoming

Definition at line 3153 of file stack/include/sl_zigbee_types.h

exchange#

uint8_t sl_zigbee_neighbor_table_entry_info_t::exchange

Definition at line 3154 of file stack/include/sl_zigbee_types.h

connectivity#

uint8_t sl_zigbee_neighbor_table_entry_info_t::connectivity

Definition at line 3157 of file stack/include/sl_zigbee_types.h

eui64#

sl_802154_long_addr_t sl_zigbee_neighbor_table_entry_info_t::eui64

Definition at line 3165 of file stack/include/sl_zigbee_types.h

mac_interface_table_index#

uint8_t sl_zigbee_neighbor_table_entry_info_t::mac_interface_table_index

Definition at line 3166 of file stack/include/sl_zigbee_types.h

lqi_for_median#

uint8_t sl_zigbee_neighbor_table_entry_info_t::lqi_for_median[3]

Definition at line 3167 of file stack/include/sl_zigbee_types.h