ZLL Commissioning Common#

API and Callbacks for the ZLL Commissioning Common Component.

Common code for the ZigBee 3.0 touchlink commissioning mechanism. This component is required for both server and client side implementations.

Modules#

Zll Commissioning Common

API#

sl_status_t

Generate a random network key and initializes the security state of the device.

bool

Indicate whether a touch link procedure is currently in progress.

void

Reset the local device to a factory new state.

sl_status_t

Disable touchlink processing.

sl_status_t

Enable touchlink processing.

Enumerations#

enum
INITIAL = 0x0000
SCAN_FOR_TOUCH_LINK = 0x0001
SCAN_FOR_DEVICE_INFORMATION = 0x0002
SCAN_FOR_IDENTIFY = 0x0004
SCAN_FOR_RESET = 0x0008
TARGET_NETWORK_FOUND = 0x0010
ABORTING_TOUCH_LINK = 0x0020
SCAN_COMPLETE = 0x0040
TOUCH_LINK_TARGET = 0x0080
FORMING_NETWORK = 0x0100
RESETTING_TO_FACTORY_NEW = 0x0200
}

Macros#

#define
touchLinkInProgress ()
#define
scanForTouchLink ()
#define
scanForDeviceInformation ()
#define
scanForIdentify ()
#define
scanForReset ()
#define
targetNetworkFound ()
#define
abortingTouchLink ()
#define
scanComplete ()
#define
touchLinkTarget ()
#define
formingNetwork ()
#define
resettingToFactoryNew ()
#define
ZLL_FRAME_CONTROL_LEGACY 0x00
#define
ZLL_FRAME_CONTROL_CLIENT_TO_SERVER 0x11
#define
ZLL_FRAME_CONTROL_SERVER_TO_CLIENT 0x19
#define
ZLL_HEADER_FRAME_CONTROL_OFFSET 0
#define
ZLL_HEADER_SEQUENCE_NUMBER_OFFSET 1
#define
ZLL_HEADER_COMMAND_ID_OFFSET 2
#define
ZLL_HEADER_TRANSACTION_ID_OFFSET 3
#define
ZLL_HEADER_OVERHEAD 7
#define
debugPrintln (...)
#define
debugPrint (...)
#define
debugExec (x)
#define
sl_zigbee_af_zll_commissioning_initial_security_state_cb sl_zigbee_af_zll_commissioning_common_initial_security_state_cb
#define
sl_zigbee_af_zll_commissioning_touch_link_complete_cb sl_zigbee_af_zll_commissioning_common_touch_link_complete_cb
#define
sl_zigbee_af_zll_commissioning_reset_to_factory_new_cb sl_zigbee_af_zll_commissioning_common_reset_to_factory_new_cb

API Documentation#

sl_zigbee_af_zll_set_initial_security_state#

sl_status_t sl_zigbee_af_zll_set_initial_security_state (void )

Generate a random network key and initializes the security state of the device.

Parameters
N/A

This function is a convenience wrapper for sl_zigbee_zll_set_initial_security_state, which must be called before starting or joining a network. The plugin initializes the security state for the initiator during touch linking. The target must initialize its own security state prior to forming a network either by using this function or by calling sl_zigbee_zll_set_initial_security_state directly.

Returns

  • An ::sl_status_t value that indicates the success or failure of the command.


Definition at line 66 of file app/framework/plugin/zll-commissioning-common/zll-commissioning-common.h

sl_zigbee_af_zll_touch_link_in_progress#

bool sl_zigbee_af_zll_touch_link_in_progress (void )

Indicate whether a touch link procedure is currently in progress.

Parameters
N/A

Returns

  • True if a touch link is in progress or false otherwise.


Definition at line 72 of file app/framework/plugin/zll-commissioning-common/zll-commissioning-common.h

sl_zigbee_af_zll_reset_to_factory_new#

void sl_zigbee_af_zll_reset_to_factory_new (void )

Reset the local device to a factory new state.

Parameters
N/A

This function causes the device to leave the network and clear its network parameters, resets its attributes to their default values, and clears the group and scene tables.


Definition at line 80 of file app/framework/plugin/zll-commissioning-common/zll-commissioning-common.h

sl_zigbee_af_zll_disable#

sl_status_t sl_zigbee_af_zll_disable (void )

Disable touchlink processing.

Parameters
N/A

This function will cause the device to refuse network start/join requests if it receives them and will not allow touchlinking. Note that this will have the effect of overriding the sl_zigbee_af_zll_no_touchlink_for_nfn function.


Definition at line 89 of file app/framework/plugin/zll-commissioning-common/zll-commissioning-common.h

sl_zigbee_af_zll_enable#

sl_status_t sl_zigbee_af_zll_enable (void )

Enable touchlink processing.

Parameters
N/A

This function will cause the device to accept network start/join requests if it receives them and will not allow touchlinking. Note that this will have the effect of overriding the sl_zigbee_af_zll_no_touchlink_for_nfn function.


Definition at line 98 of file app/framework/plugin/zll-commissioning-common/zll-commissioning-common.h

Enumeration Documentation#

StateEnum#

StateEnum
Enumerator
INITIAL
SCAN_FOR_TOUCH_LINK
SCAN_FOR_DEVICE_INFORMATION
SCAN_FOR_IDENTIFY
SCAN_FOR_RESET
TARGET_NETWORK_FOUND
ABORTING_TOUCH_LINK
SCAN_COMPLETE
TOUCH_LINK_TARGET
FORMING_NETWORK
RESETTING_TO_FACTORY_NEW

Definition at line 184 of file app/framework/plugin/zll-commissioning-common/zll-commissioning-common.h

Variable Documentation#

sli_zigbee_af_zll_network#

sl_zigbee_zll_network_t sli_zigbee_af_zll_network

Definition at line 165 of file app/framework/plugin/zll-commissioning-common/zll-commissioning-common.h

sli_zigbee_af_zll_flags#

uint16_t sli_zigbee_af_zll_flags

Definition at line 166 of file app/framework/plugin/zll-commissioning-common/zll-commissioning-common.h

sli_zigbee_af_initiator_rejoin_retry_count#

uint8_t sli_zigbee_af_initiator_rejoin_retry_count

Definition at line 167 of file app/framework/plugin/zll-commissioning-common/zll-commissioning-common.h