Defines a ZigBee network and the associated parameters.
Public Attribute Documentation#
panId#
uint16_t sl_zigbee_zigbee_network_t::panId
channel#
uint8_t sl_zigbee_zigbee_network_t::channel
allowingJoin#
bool sl_zigbee_zigbee_network_t::allowingJoin
extendedPanId#
uint8_t sl_zigbee_zigbee_network_t::extendedPanId[EXTENDED_PAN_ID_SIZE]
stackProfile#
uint8_t sl_zigbee_zigbee_network_t::stackProfile
nwkUpdateId#
uint8_t sl_zigbee_zigbee_network_t::nwkUpdateId