You are viewing documentation for version: 4.2 | Version History ... Configuration Options The API Flow Control Support Example ... // Set to 1 to enable hardware flow control.
ProductMicrocontrollersResource TypeSoftware API documentation
Home ... // Gecko Platform//Version 4.4.1 //Services //API Documentation //Sleep Timer ... All API functions can be called from within interrupt handlers. ... Expected value: 1-31. uint8_t N/A
// Platform//Version 5.0.1 //Security //API Documentation //SE Manager ... example the device will erase OTP and become inoperable if 4 glitch signals is seen in a 1 minute time period.