... and supports multiple driver instances. The driver does not buffer or queue data. However, it queues UART ... A receiver should set RTS high when it is no longer capable of receiving data.
ProductMicrocontrollersResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... A pointer to this function is passed to sl_sleeptimer_start_timer().
RTT module uses a control block structure located in RAM memory with a specific ID so that it can be discovered ... Functions sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables
ProductMicrocontrollersResource TypeSoftware API documentation
Results 1-6 of 6 for gecko-platform/3.0/emlib/api/efm32tg11/driver/api/struct-u-a-r-t-d-r-v-init-euart-t