Configuration Options The API Flow Control Support Example ... Query the status of a current transmit or receive operations. ... [in] callback A transfer completion callback. Returns
ProductMicrocontrollersResource TypeSoftware API documentation
// Platform//Version 5.0.1 //Security //API Documentation //SE Manager ... is the recommended device independent crypto API and should be used whenever possible. ... Description 0 Ignore
You are viewing documentation for version: 4.2 | Version History ... Overview ... Functions sl_status_t sl_iostream_rtt_init (void) ... Returns Status result Variable Documentation
ProductMicrocontrollersResource TypeSoftware API documentation
... , my_timer_callback, (void *)NULL, 0, 0); if(status != SL_STATUS_OK) { return -1; } return 1; } ... N/A callback Callback function that will be called when initial/periodic timeout expires.
Results 1-6 of 6 for gecko-platform/3.0/emlib/api/efm32tg11/middleware/api/group-usbx-callback-status