Silicon Labs
gecko-platform/3.0/emlib/api/efm32xg1/middleware/api/struct-u-s-b-x-init-t
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
Results 1-5 of 5 for gecko-platform/3.0/emlib/api/efm32xg1/middleware/api/struct-u-s-b-x-init-t in 0.18 seconds
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
Driver for the Bosch Sensortec BMP280 barometric pressure sensor ... Driver for the Silicon Labs Si7210 Hall effect sensor ... Platform Services Detail Device Initialization
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
// Gecko Platform//Version 4.4.1 //Services ... The hardware timer peripheral must be properly clocked from the application. ... All API functions can be called from within interrupt handlers.
UARTDRV - UART Driver - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-uart...
... hardware flow control on devices that don't have UART CTS/RTS hardware support, the driver includes the GPIOINT driver to emulate a hardware implementation of UART CTS/RTS flow control on ...
ProductMicrocontrollers Resource TypeSoftware API documentation
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Hardware block inside the SE used for generating random numbers.
I/O Stream RTT - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-iostream-...
You should avoid using it in production. ... sl_iostream_rtt_handle sl_iostream_instance_info_t sl_iostream_instance_rtt_info ... sl_iostream_instance_info_t sl_iostream_instance_rtt_info
ProductMicrocontrollers Resource TypeSoftware API documentation
    Results 1-5 of 5 for gecko-platform/3.0/emlib/api/efm32xg1/middleware/api/struct-u-s-b-x-init-t