Silicon Labs
gecko-platform/3.0/emlib/api/efr32xg21/service/api/structsl-sleeptimer-timer-handle
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
    Results 1-5 of 5 for gecko-platform/3.0/emlib/api/efr32xg21/service/api/structsl-sleeptimer-timer-handle in 0.18 seconds
    System | Bluetooth API Reference Guide | Bluetooth LE | v6.1.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-sys...
    // Bluetooth LE//Version 6.1.0 //Bluetooth API Reference Guide //System ... sl_bt_rsp_system_data_buffer_write_id 0x12010020 ... Bluetooth identity address in little endian format
    Resource TypeSoftware API Documentation
    System | Bluetooth API Reference Guide | Bluetooth LE | v6.0.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-sys...
    // Bluetooth LE//Version 6.0.0 //Bluetooth API Reference Guide //System ... sl_bt_rsp_system_data_buffer_write_id 0x12010020 ... Bluetooth identity address in little endian format
    Resource TypeSoftware API Documentation
    GATT Server | GATT Server | Bluetooth LE | v3.2 | Silicon Labs
    https://docs.silabs.com/....
    Write the value of an attribute in the local GATT database. ... parameter att_opcode in the event is sl_bt_gatt_write_request or sl_bt_gatt_execute_write_request (see sl_bt_gatt_att_opcode_t).
    Connection | Bluetooth Stack API Reference | Bluetooth LE | v8.1.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-connect...
    // Bluetooth LE//Version 8.1.0 //Bluetooth Stack API Reference //Connection ... sl_bt_rsp_connection_set_remote_power_reporting_id 0x0a060020 ... Size of output buffer passed in channel_map
    Advertiser | Bluetooth Stack API Reference | Bluetooth LE | v8.0.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-adverti...
    // Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... sl_bt_rsp_advertiser_clear_random_address_id 0x11040020 ... Time range: 10 ms to 655.35 s Default : 0 uint8_t
      Results 1-5 of 5 for gecko-platform/3.0/emlib/api/efr32xg21/service/api/structsl-sleeptimer-timer-handle