The Bluetooth SDK comes with a number of example application that you can then modify to create your own ... SDK may be installed manually by downloading or cloning the latest from GitHub.
// Bluetooth LE//Version 3.3 //Lab Manuals ... Ensure that the Secure Firmware Version is the latest one. ... Select Bluetooth - SoC Empty from the Bluetooth examples and click Create.
// Bluetooth LE//Version 2.13 //API Reference ... Errors related to hardware# ... Errors from Attribute Protocol Bluetooth Mesh errors Bluetooth Mesh foundation errors Filesystem errors
5.3.0 Bluetooth NCP Commander# Bluetooth NCP Commander is a Simplicity Studio® 5 (SSv5) tool for sending BGAPI ... Table of Contents Bluetooth NCP Commander Bluetooth NCP Commander Standalone
ProductSimplicity StudioResource TypeSoftware API Documentation
Training ... Register // Bluetooth LE//Version 9.0.0 //Developer's Guide ... 9.0.0 Bluetooth LE Developers Guide# The Developer's Guide content is organized in the following groups:
Results 1-5 of 5 for gecko-platform/3.1/emlib/api/efm32gg12/driver/api/group-spidrv