Description Version API. Macros specifying the EMLIB and CMSIS version. ... #define _EMLIB_VERSION_PATCH 0 #define _CMSIS_VERSION 5.3.0 Version number of targeted CMSIS package.
ProductMicrocontrollersResource TypeSoftware API documentation
5.1.2 (latest) Platform# Platform (formerly known as Gecko Platform) is the foundation for Silicon Labs ... Gecko SDK will continue to be available providing long-term support for our Series 0 ...
Configuration Options The API Flow Control Support Example ... // Set to 1 to enable hardware flow control. ... uartdrvAbortTransmit = 1, uartdrvAbortReceive = 2, uartdrvAbortAll = 3
ProductMicrocontrollersResource TypeSoftware API documentation
Training ... Github ... // Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... http://man7.org/linux/man-pages/man3/strftime.3.html
... open a telnet session and connect to the port 19021 using your host IP address when the debugger is connected using USB and using J-Link debugger IP address when your debugger is connected ...
ProductMicrocontrollersResource TypeSoftware API documentation
Results 1-6 of 6 for gecko-platform/3.1/emlib/api/efm32hg/middleware/api/group-usb-host