Training ... Github ... // Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... http://man7.org/linux/man-pages/man3/strftime.3.html
// Platform//Version 5.0.1 //Security ... is the recommended device independent crypto API and should be used whenever possible. ... The SETAMPERHOST interrupt on the host is triggered.
... open a telnet session and connect to the port 19021 using your host IP address when the debugger is connected using USB and using J-Link debugger IP address when your debugger is connected ...
ProductMicrocontrollersResource TypeSoftware API documentation
Configuration Options The API Flow Control Support Example ... // Set to 1 to enable hardware flow control. ... uartdrvAbortTransmit = 1, uartdrvAbortReceive = 2, uartdrvAbortAll = 3
ProductMicrocontrollersResource TypeSoftware API documentation
3.1 SimEEv1/v2 SimEEv1/v2 can be used with EmberZNet PRO and Silicon Labs Connect ( ... 3.2 PS Store PS Store can be used with Bluetooth devices on all platforms except for ... 36 KB 3 8 KB
Resource TypeUser's Guides
Results 1-6 of 6 for gecko-platform/3.1/emlib/api/efm32tg/middleware/api/group-usb-device