Description Version API. Macros specifying the EMLIB and CMSIS version. ... #define _EMLIB_VERSION_PATCH 0 #define _CMSIS_VERSION 5.3.0 Version number of targeted CMSIS package.
ProductMicrocontrollersResource TypeSoftware API documentation
5.1.2 (latest) Platform# Platform (formerly known as Gecko Platform) is the foundation for Silicon Labs ... Gecko SDK will continue to be available providing long-term support for our Series 0 ...
Configuration Options The API Flow Control Support ... // Set to 1 to enable hardware flow control. ... and RTS locations by setting portLocationCts and portLocationRts in the init struct.
ProductMicrocontrollersResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... 0 if successful. Error code otherwise. sl_sleeptimer_restart_periodic_timer#
RTT module uses a control block structure located in RAM memory with a specific ID so that it can be discovered when a connection is established via J-Link. ... sl_iostream_instance_rtt_info
ProductMicrocontrollersResource TypeSoftware API documentation
Results 1-6 of 6 for gecko-platform/3.1/emlib/api/efr32xg21/driver/api/group-driver