Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... dms_claim <dms_token> The Gecko DMS Commands When using Gecko OS, DMS commands is ... ls
ProductWirelessResource TypeSoftware API documentation
... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren )
ProductWirelessResource TypeSoftware API documentation
The Gecko OS Command API is friendly for humans too. ... dms_activate <product code> [ update /-o / -m] ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ...
Results 1-5 of 5 for gecko-platform/3.2/emlib/api/efm32g/service/api/group-iostream