... that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... , secure boot and secure debug implementation, is available on all series 2 devices.
2.This signature is the final argument of the Debug Unlock Token. ... 3.If DBGLOCK is unlocked, the NIDLOCK should also be unlocked. ... 2.These APIs are only available on HSE devices.
Resource TypeApplication Notes
Results 1-6 of 6 for gecko-platform/3.2/emlib/api/efm32g/service/api/group-iostream-leuart