RTT module uses a control block structure located in RAM memory with a specific ID so that it can be ... sl_iostream_rtt_handle sl_iostream_t * sl_iostream_rtt_handle sl_iostream_rtt_handle
ProductMicrocontrollersResource TypeSoftware API documentation
You are viewing documentation for version: 3.1 | Version History ... This file contains the glue logic between the mbed TLS threading API and two RTOS'es supported, being Micrium OS and ...
ProductMicrocontrollersResource TypeSoftware API documentation
... that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... , secure boot and secure debug implementation, is available on all series 2 devices.
You are viewing documentation for version: 4.2 | Version History ... Configuration Options The API Flow Control Support ... Both blocking and non-blocking transfer functions are available.
ProductMicrocontrollersResource TypeSoftware API documentation
Training ... Github ... // Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... http://man7.org/linux/man-pages/man3/strftime.3.html
Results 1-6 of 6 for gecko-platform/3.2/emlib/api/efm32gg/service/api/group-iostream-rtt