SWO Debug
Description
Serial Wire Output Debug Configuration.
Initializes Serial Wire Output using the DWT and ITM peripherals of Cortex-M processors. Configures output of Program Counter samples, interrupt events, and data over any ITM channel.
Functions | |
sl_status_t | sl_debug_swo_init (void) |
Initialize SWO Debug. | |
sl_status_t | sl_debug_swo_enable_itm (uint32_t channel) |
Enable an ITM channel. | |
sl_status_t | sl_debug_swo_disable_itm (uint32_t channel) |
Disable an ITM channel. | |
sl_status_t | sl_debug_swo_write (uint32_t channel, uint8_t c) |
Write a byte to an ITM channel. | |
Function Documentation
◆ sl_debug_swo_init()
sl_status_t sl_debug_swo_init | ( | void |
| ) |
Initialize SWO Debug.
Initializes SWO debug using configuration parameters for frequency, as well as whether PC sample events and interrupt events should be emitted.
- Note
- This function does not enable any software stimulus ports in the ITM. This can be done by calling sl_debug_swo_enable_itm or by using sl_debug_swo_write which enables the necessary ports automatically.
- Returns
- Status code
- Return values
-
SL_STATUS_OK
SWO initialized successfully
◆ sl_debug_swo_enable_itm()
sl_status_t sl_debug_swo_enable_itm | ( | uint32_t | channel | ) |
Enable an ITM channel.
Enables the given ITM channel in the Trace Enable Register.
- Parameters
-
[in] channel
ITM channel number
- Returns
- Status code
- Return values
-
SL_STATUS_OK
ITM channel enabled successfully
◆ sl_debug_swo_disable_itm()
sl_status_t sl_debug_swo_disable_itm | ( | uint32_t | channel | ) |
Disable an ITM channel.
Disables the given ITM channel in the Trace Enable Register.
- Parameters
-
[in] channel
ITM channel number
- Returns
- Status code
- Return values
-
SL_STATUS_OK
ITM channel disabled successfully
◆ sl_debug_swo_write()
sl_status_t sl_debug_swo_write | ( | uint32_t | channel, |
uint8_t | c |
||
) |
Write a byte to an ITM channel.
Writes the given byte to the given ITM channel
- Note
- This function ensures that the ITM channel is enabled, and enables it if it wasn't already.
- Parameters
-
[in] channel
ITM channel number [in] c
Byte to send
- Returns
- Status code
- Return values
-
SL_STATUS_OK
Byte sent successfully SL_STATUS_NOT_INITIALIZED
ITM has not been enabled, call sl_debug_swo_init first.