sl_button_t Struct Reference
A BUTTON instance.
#include <sl_button.h>
Data Fields | |
void * | context |
The context for this BUTTON instance. | |
sl_status_t(* | init )(void *context) |
Member function to initialize BUTTON instance. | |
void(* | poll )(void *context) |
Member function to poll BUTTON. | |
void(* | enable )(void *context) |
Member function to enable BUTTON. | |
void(* | disable )(void *context) |
Member function to disable BUTTON. | |
sl_button_state_t(* | get_state )(void *context) |
Member function to retrieve BUTTON state. | |
A BUTTON instance.
Field Documentation
◆ context
void* sl_button_t::context |
The context for this BUTTON instance.
◆ init
sl_status_t(* sl_button_t::init) (void *context) |
Member function to initialize BUTTON instance.
◆ poll
void(* sl_button_t::poll) (void *context) |
Member function to poll BUTTON.
◆ enable
void(* sl_button_t::enable) (void *context) |
Member function to enable BUTTON.
◆ disable
void(* sl_button_t::disable) (void *context) |
Member function to disable BUTTON.
◆ get_state
sl_button_state_t(* sl_button_t::get_state) (void *context) |
Member function to retrieve BUTTON state.