sl_pwm_instance Struct Reference
PWM driver instance.
#include <sl_pwm.h>
Data Fields | |
TIMER_TypeDef * | timer |
TIMER instance. | |
uint8_t | channel |
TIMER channel. | |
uint8_t | port |
GPIO port. | |
uint8_t | pin |
GPIO pin. | |
uint8_t | location |
GPIO location. | |
PWM driver instance.
Field Documentation
◆ timer
TIMER_TypeDef* sl_pwm_instance::timer |
TIMER instance.
◆ channel
uint8_t sl_pwm_instance::channel |
TIMER channel.
◆ port
uint8_t sl_pwm_instance::port |
GPIO port.
◆ pin
uint8_t sl_pwm_instance::pin |
GPIO pin.
◆ location
uint8_t sl_pwm_instance::location |
GPIO location.