HFRCO Initialization
Description
Initialize the HFRCO oscillator.
Configure the frequency band of the HFRCO. The configuration define SL_DEVICE_INIT_HFRCO_BAND is used to configure the frequency.
Functions | |
sl_status_t | sl_device_init_hfrco (void) |
Initialize HFRCO. | |
Function Documentation
◆ sl_device_init_hfrco()
sl_status_t sl_device_init_hfrco | ( | void |
| ) |
Initialize HFRCO.
Configure the frequency band of the HFRCO. The configuration define SL_DEVICE_INIT_HFRCO_BAND is used to configure the frequency.
- Returns
- Status code
- Return values
-
SL_STATUS_OK
HFRCO initialized successfully