NVIC Initialization
Description
Initialize the NVIC Interrupt Handlers priority.
Set all interrupt priorities, except the Fault exceptions, to CORE_INTERRUPT_DEFAULT_PRIORITY
value.
When the Device Init NVIC module is present and no configuration overwrites the em_core CORE_ATOMIC_METHOD
define, the atomic method is automatically set to BASEPRI (CORE_ATOMIC_METHOD_BASEPRI
).
Functions | |
sl_status_t | sl_device_init_nvic (void) |
Sets default priority for all configurable interrupts in NVIC. | |
Function Documentation
◆ sl_device_init_nvic()
sl_status_t sl_device_init_nvic | ( | void |
| ) |
Sets default priority for all configurable interrupts in NVIC.
- Returns
- Status code