Key handling
Description
Secure Engine key handling API.
API for using cryptographic keys with the SE. Contains functionality to generate, import and export keys to and from protected types like wrapped or volatile keys.
Data Structures | |
struct | sl_se_buffer_t |
Describes where the key is or should be stored. | |
struct | sl_se_key_storage_t |
Describes the storage location of keys. | |
struct | sl_se_key_descriptor_t |
Contains a full description of a key used by an SE command. | |
struct | sl_se_custom_weierstrass_prime_domain_t |
Custom Weierstrass curve structure. | |
Functions | |
sl_status_t | sl_se_validate_key (const sl_se_key_descriptor_t *key) |
Validate key descriptor. | |
sl_status_t | sl_se_generate_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_out) |
Generate a random key adhering to the given key descriptor. | |
sl_status_t | sl_se_import_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_in, const sl_se_key_descriptor_t *key_out) |
Import a key using the SE. | |
sl_status_t | sl_se_export_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_in, const sl_se_key_descriptor_t *key_out) |
Export a volatile or wrapped key back to plaintext. | |
sl_status_t | sl_se_transfer_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_in, const sl_se_key_descriptor_t *key_out) |
Transfer a volatile or wrapped key to another protected storage. | |
sl_status_t | sl_se_export_public_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key_in, const sl_se_key_descriptor_t *key_out) |
Export the public part of an ECC keypair. | |
sl_status_t | sl_se_delete_key (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key) |
Delete a key from a volatile SE storage slot. | |
sl_status_t | sl_se_get_storage_size (const sl_se_key_descriptor_t *key, uint32_t *storage_size) |
Returns the required storage size for the given key. | |
Macros | |
#define | SL_SE_KEY_FLAG_ASYMMETRIC_SIGNING_ONLY (1UL << 10) |
Asymmetric key can only be used for signing (not key exchange) | |
#define | SL_SE_KEY_FLAG_ASYMMETRIC_USES_CUSTOM_DOMAIN (1UL << 12) |
Described key belongs to a custom ECC domain. | |
#define | SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PUBLIC_KEY (1UL << 13) |
Storage buffer contains public part of an asymmetric key. | |
#define | SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PRIVATE_KEY (1UL << 14) |
Storage buffer contains private part of an asymmetric key. | |
#define | SL_SE_KEY_FLAG_ALLOW_ANY_ACCESS (1UL << 15) |
Allow usage of this key by other bus masters or TrustZone levels than the one which created/imported the key. | |
#define | SL_SE_KEY_FLAG_ASYMMMETRIC_SIGNING_ONLY (SL_SE_KEY_FLAG_ASYMMETRIC_SIGNING_ONLY) |
Old definition. Retained for backwards compatibility. | |
#define | SL_SE_KEY_FLAG_NON_EXPORTABLE (1UL << 24) |
Do not allow exporting the key to plaintext. | |
#define | SL_SE_KEY_FLAG_IS_DEVICE_GENERATED (1UL << 25) |
Indicate that the key has been generated by this device. | |
#define | SL_SE_KEY_FLAG_IS_RESTRICTED (1UL << 25 | 1UL << 24) |
Indicate that the key can only be used to sign SE generated content. | |
#define | SL_SE_KEY_TYPE_ALGORITHM_MASK 0xf0000000 |
Mask for algorithm field in key type. | |
#define | SL_SE_KEY_TYPE_ALGORITHM_OFFSET 28 |
Offset of algorithm field in key type. | |
#define | SL_SE_KEY_TYPE_ATTRIBUTES_MASK 0x00007fff |
Mask for attributes field in key type. | |
#define | SL_SE_KEY_TYPE_ATTRIBUTES_OFFSET 0 |
Offset of attributes field in key type. | |
#define | SL_SE_KEY_TYPE_SYMMETRIC 0x00000000 |
Symmetric key type. | |
#define | SL_SE_KEY_TYPE_AES_128 0x00000010 |
Symmetric key type for AES-128 (16 byte key) | |
#define | SL_SE_KEY_TYPE_AES_192 0x00000018 |
Symmetric key type for AES-192 (24 byte key) | |
#define | SL_SE_KEY_TYPE_AES_256 0x00000020 |
Symmetric key type for AES-256 (32 byte key) | |
#define | SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM (0x8U << SL_SE_KEY_TYPE_ALGORITHM_OFFSET) |
ECC Weierstrass Prime key type. | |
#define | SL_SE_KEY_TYPE_ECC_P192 (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x18)) |
ECC NIST P-192. | |
#define | SL_SE_KEY_TYPE_ECC_P224 (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x1C)) |
ECC NIST P-224. | |
#define | SL_SE_KEY_TYPE_ECC_P256 (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x20)) |
ECC NIST P-256. | |
#define | SL_SE_KEY_TYPE_CHACHA20 0x00000020 |
Symmetric key type for ChaCha20. | |
#define | SL_SE_KEY_TYPE_ECC_MONTGOMERY (0xbU << SL_SE_KEY_TYPE_ALGORITHM_OFFSET) |
ECC Montgomery key type. | |
#define | SL_SE_KEY_TYPE_ECC_EDDSA (0xcU << SL_SE_KEY_TYPE_ALGORITHM_OFFSET) |
EDDSA key type. | |
#define | SL_SE_KEY_TYPE_ECC_P384 (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x30)) |
ECC NIST P-384. | |
#define | SL_SE_KEY_TYPE_ECC_P521 (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x42)) |
ECC NIST P-521. | |
#define | SL_SE_KEY_TYPE_ECC_X25519 (SL_SE_KEY_TYPE_ECC_MONTGOMERY | (0x20)) |
ECC X25519 key for ECDH. | |
#define | SL_SE_KEY_TYPE_ECC_X448 (SL_SE_KEY_TYPE_ECC_MONTGOMERY | (0x38)) |
ECC X448 key for ECDH. | |
#define | SL_SE_KEY_TYPE_ECC_ED25519 (SL_SE_KEY_TYPE_ECC_EDDSA | (0x20)) |
ECC Ed25519 key for EdDSA. | |
#define | SL_SE_KEY_TYPE_ECC_ED448 (SL_SE_KEY_TYPE_ECC_EDDSA | (0x38)) |
ECC Ed448 key for EdDSA. | |
#define | SL_SE_KEY_STORAGE_EXTERNAL_PLAINTEXT 0x00 |
Key storage methods. | |
#define | SL_SE_KEY_STORAGE_EXTERNAL_WRAPPED 0x01 |
Key is stored encrypted in application memory. | |
#define | SL_SE_KEY_STORAGE_INTERNAL_VOLATILE 0x02 |
Key is stored inside the SE, and will persist until system reset or explicitly deleted. | |
#define | SL_SE_KEY_STORAGE_INTERNAL_IMMUTABLE 0x03 |
Key is one of the pre-defined keys (pre-loaded or write-once) available in the SE. | |
#define | SL_SE_KEY_SLOT_VOLATILE_0 0x00 |
List of available internal SE key slots. | |
#define | SL_SE_KEY_SLOT_VOLATILE_1 0x01 |
Internal volatile slot 1. | |
#define | SL_SE_KEY_SLOT_VOLATILE_2 0x02 |
Internal volatile slot 2. | |
#define | SL_SE_KEY_SLOT_VOLATILE_3 0x03 |
Internal volatile slot 3. | |
#define | SL_SE_KEY_SLOT_APPLICATION_SECURE_DEBUG_KEY 0xF8 |
Internal immutable application secure debug key. | |
#define | SL_SE_KEY_SLOT_APPLICATION_AES_128_KEY 0xFA |
Internal immutable application AES-128 key (bootloader key) | |
#define | SL_SE_KEY_SLOT_APPLICATION_SECURE_BOOT_KEY 0xFC |
Internal immutable application secure boot key. | |
#define | SL_SE_KEY_SLOT_APPLICATION_ATTESTATION_KEY 0xFE |
Internal immutable application attestation key. | |
#define | SL_SE_KEY_SLOT_SE_ATTESTATION_KEY 0xFF |
Internal immutable SE attestation key. | |
#define | SLI_SE_WRAPPED_KEY_OVERHEAD (12 + 16) |
Size overhead for wrapped keys. | |
Typedefs | |
typedef uint32_t | sl_se_key_type_t |
Supported key types. | |
typedef uint32_t | sl_se_storage_method_t |
Key storage method. | |
typedef uint32_t | sl_se_key_slot_t |
Internal SE key slot. | |
Function Documentation
◆ sl_se_validate_key()
sl_status_t sl_se_validate_key | ( | const sl_se_key_descriptor_t * | key | ) |
Validate key descriptor.
Takes a key descriptor and checks if all required properties have been set for the specific key type.
- Parameters
-
[in] key
The key to validate.
- Returns
- Status code, sl_status.h.
◆ sl_se_generate_key()
sl_status_t sl_se_generate_key | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key_out |
||
) |
Generate a random key adhering to the given key descriptor.
The SE takes a key descriptor and generates a key with the given properties in the location specified by the descriptor.
If the key size is not aligned to a multiple of words the key representation is padded in front of the key.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key_out
Description of the key to generate. Sets key parameters and describes the storage location for the key.
- Returns
- Status code, sl_status.h.
◆ sl_se_import_key()
sl_status_t sl_se_import_key | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key_in, |
||
const sl_se_key_descriptor_t * | key_out |
||
) |
Import a key using the SE.
Protect a key using the SE. Import a plaintext key and store it either in a volatile slot or as a wrapped key.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key_in
A plaintext key. [in] key_out
Either a volatile or a wrapped key with similar properties as key_in.
- Returns
- Status code, sl_status.h.
◆ sl_se_export_key()
sl_status_t sl_se_export_key | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key_in, |
||
const sl_se_key_descriptor_t * | key_out |
||
) |
Export a volatile or wrapped key back to plaintext.
Attempt to have the SE export a volatile or wrapped key back to plaintext if allowed.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key_in
Either a volatile or a wrapped key with similar properties as key_out. [in] key_out
The exported key in plaintext.
- Returns
- Status code, sl_status.h. SL_STATUS_INVALID_PARAMETER if key does not exist.
◆ sl_se_transfer_key()
sl_status_t sl_se_transfer_key | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key_in, |
||
const sl_se_key_descriptor_t * | key_out |
||
) |
Transfer a volatile or wrapped key to another protected storage.
Attempt to have the SE transfer a volatile or wrapped key if allowed.
- Note
- The key stored in the source protected storage will not be deleted.
Transferring a key between the same volatile slot is not allowed.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key_in
Either a volatile or a wrapped key with similar properties as key_out. [in] key_out
Either a volatile or a wrapped key with similar properties as key_in.
- Returns
- Status code, sl_status.h. SL_STATUS_INVALID_PARAMETER if key does not exist.
◆ sl_se_export_public_key()
sl_status_t sl_se_export_public_key | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key_in, |
||
const sl_se_key_descriptor_t * | key_out |
||
) |
Export the public part of an ECC keypair.
The output key must be specified to only contain a public key.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key_in
An asymmetric key with either a private or public part. [out] key_out
Describes output key parameters. Should only be set to contain the public part of the key.
- Returns
- Status code, sl_status.h.
◆ sl_se_delete_key()
sl_status_t sl_se_delete_key | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key |
||
) |
Delete a key from a volatile SE storage slot.
The given key will be removed from the SE. The key descriptor is not modified and can be used to generate a new key without any updates.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Key to delete.
- Returns
- Status code, sl_status.h.
◆ sl_se_get_storage_size()
sl_status_t sl_se_get_storage_size | ( | const sl_se_key_descriptor_t * | key, |
uint32_t * | storage_size |
||
) |
Returns the required storage size for the given key.
Finds the total storage size required for a given key. This includes storage for the public and private part of asymmetric keys, as well as overhead for wrapping keys.
- Parameters
-
[in] key
The sl_se_key_descriptor_t to find the required storage size for. [out] storage_size
The required storage size in bytes.
- Returns
- Status code, sl_status.h.
Macro Definition Documentation
◆ SL_SE_KEY_FLAG_ASYMMETRIC_SIGNING_ONLY
#define SL_SE_KEY_FLAG_ASYMMETRIC_SIGNING_ONLY (1UL << 10) |
Asymmetric key can only be used for signing (not key exchange)
◆ SL_SE_KEY_FLAG_ASYMMETRIC_USES_CUSTOM_DOMAIN
#define SL_SE_KEY_FLAG_ASYMMETRIC_USES_CUSTOM_DOMAIN (1UL << 12) |
Described key belongs to a custom ECC domain.
◆ SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PUBLIC_KEY
#define SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PUBLIC_KEY (1UL << 13) |
Storage buffer contains public part of an asymmetric key.
◆ SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PRIVATE_KEY
#define SL_SE_KEY_FLAG_ASYMMETRIC_BUFFER_HAS_PRIVATE_KEY (1UL << 14) |
Storage buffer contains private part of an asymmetric key.
◆ SL_SE_KEY_FLAG_ALLOW_ANY_ACCESS
#define SL_SE_KEY_FLAG_ALLOW_ANY_ACCESS (1UL << 15) |
Allow usage of this key by other bus masters or TrustZone levels than the one which created/imported the key.
◆ SL_SE_KEY_FLAG_ASYMMMETRIC_SIGNING_ONLY
#define SL_SE_KEY_FLAG_ASYMMMETRIC_SIGNING_ONLY (SL_SE_KEY_FLAG_ASYMMETRIC_SIGNING_ONLY) |
Old definition. Retained for backwards compatibility.
◆ SL_SE_KEY_FLAG_NON_EXPORTABLE
#define SL_SE_KEY_FLAG_NON_EXPORTABLE (1UL << 24) |
Do not allow exporting the key to plaintext.
◆ SL_SE_KEY_FLAG_IS_DEVICE_GENERATED
#define SL_SE_KEY_FLAG_IS_DEVICE_GENERATED (1UL << 25) |
Indicate that the key has been generated by this device.
This flag is only valid when using the SE to generate a key and makes it non-exportable.
◆ SL_SE_KEY_FLAG_IS_RESTRICTED
#define SL_SE_KEY_FLAG_IS_RESTRICTED (1UL << 25 | 1UL << 24) |
Indicate that the key can only be used to sign SE generated content.
This flag is only valid when using the SE to generate a key and makes it non-exportable.
◆ SL_SE_KEY_TYPE_ALGORITHM_MASK
#define SL_SE_KEY_TYPE_ALGORITHM_MASK 0xf0000000 |
Mask for algorithm field in key type.
◆ SL_SE_KEY_TYPE_ALGORITHM_OFFSET
#define SL_SE_KEY_TYPE_ALGORITHM_OFFSET 28 |
Offset of algorithm field in key type.
◆ SL_SE_KEY_TYPE_ATTRIBUTES_MASK
#define SL_SE_KEY_TYPE_ATTRIBUTES_MASK 0x00007fff |
Mask for attributes field in key type.
◆ SL_SE_KEY_TYPE_ATTRIBUTES_OFFSET
#define SL_SE_KEY_TYPE_ATTRIBUTES_OFFSET 0 |
Offset of attributes field in key type.
◆ SL_SE_KEY_TYPE_SYMMETRIC
#define SL_SE_KEY_TYPE_SYMMETRIC 0x00000000 |
Symmetric key type.
◆ SL_SE_KEY_TYPE_AES_128
#define SL_SE_KEY_TYPE_AES_128 0x00000010 |
Symmetric key type for AES-128 (16 byte key)
◆ SL_SE_KEY_TYPE_AES_192
#define SL_SE_KEY_TYPE_AES_192 0x00000018 |
Symmetric key type for AES-192 (24 byte key)
◆ SL_SE_KEY_TYPE_AES_256
#define SL_SE_KEY_TYPE_AES_256 0x00000020 |
Symmetric key type for AES-256 (32 byte key)
◆ SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM
#define SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM (0x8U << SL_SE_KEY_TYPE_ALGORITHM_OFFSET) |
ECC Weierstrass Prime key type.
◆ SL_SE_KEY_TYPE_ECC_P192
#define SL_SE_KEY_TYPE_ECC_P192 (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x18)) |
ECC NIST P-192.
◆ SL_SE_KEY_TYPE_ECC_P224
#define SL_SE_KEY_TYPE_ECC_P224 (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x1C)) |
ECC NIST P-224.
◆ SL_SE_KEY_TYPE_ECC_P256
#define SL_SE_KEY_TYPE_ECC_P256 (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x20)) |
ECC NIST P-256.
◆ SL_SE_KEY_TYPE_CHACHA20
#define SL_SE_KEY_TYPE_CHACHA20 0x00000020 |
Symmetric key type for ChaCha20.
◆ SL_SE_KEY_TYPE_ECC_MONTGOMERY
#define SL_SE_KEY_TYPE_ECC_MONTGOMERY (0xbU << SL_SE_KEY_TYPE_ALGORITHM_OFFSET) |
ECC Montgomery key type.
◆ SL_SE_KEY_TYPE_ECC_EDDSA
#define SL_SE_KEY_TYPE_ECC_EDDSA (0xcU << SL_SE_KEY_TYPE_ALGORITHM_OFFSET) |
EDDSA key type.
◆ SL_SE_KEY_TYPE_ECC_P384
#define SL_SE_KEY_TYPE_ECC_P384 (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x30)) |
ECC NIST P-384.
◆ SL_SE_KEY_TYPE_ECC_P521
#define SL_SE_KEY_TYPE_ECC_P521 (SL_SE_KEY_TYPE_ECC_WEIERSTRASS_PRIME_CUSTOM | (0x42)) |
ECC NIST P-521.
◆ SL_SE_KEY_TYPE_ECC_X25519
#define SL_SE_KEY_TYPE_ECC_X25519 (SL_SE_KEY_TYPE_ECC_MONTGOMERY | (0x20)) |
ECC X25519 key for ECDH.
◆ SL_SE_KEY_TYPE_ECC_X448
#define SL_SE_KEY_TYPE_ECC_X448 (SL_SE_KEY_TYPE_ECC_MONTGOMERY | (0x38)) |
ECC X448 key for ECDH.
◆ SL_SE_KEY_TYPE_ECC_ED25519
#define SL_SE_KEY_TYPE_ECC_ED25519 (SL_SE_KEY_TYPE_ECC_EDDSA | (0x20)) |
ECC Ed25519 key for EdDSA.
◆ SL_SE_KEY_TYPE_ECC_ED448
#define SL_SE_KEY_TYPE_ECC_ED448 (SL_SE_KEY_TYPE_ECC_EDDSA | (0x38)) |
ECC Ed448 key for EdDSA.
◆ SL_SE_KEY_STORAGE_EXTERNAL_PLAINTEXT
#define SL_SE_KEY_STORAGE_EXTERNAL_PLAINTEXT 0x00 |
Key storage methods.
Key is stored in a plaintext buffer in application memory. Application can save its in-memory buffer to non-volatile memory as needed to provide key persistence.
◆ SL_SE_KEY_STORAGE_EXTERNAL_WRAPPED
#define SL_SE_KEY_STORAGE_EXTERNAL_WRAPPED 0x01 |
Key is stored encrypted in application memory.
This ensures the key in wrapped form is only usable on a specific device. If the key additionally needs to be prevented from ever being output as plaintext, also set the corresponding permission bit. Application can save its in-memory buffer to non-volatile memory as needed to provide key persistence. Keys stored in this way should use the flag SL_SE_KEY_FLAG_NON_EXPORTABLE unless there is a specific need to access the key value outside the SE.
◆ SL_SE_KEY_STORAGE_INTERNAL_VOLATILE
#define SL_SE_KEY_STORAGE_INTERNAL_VOLATILE 0x02 |
Key is stored inside the SE, and will persist until system reset or explicitly deleted.
Keys stored in this way should use the flag SL_SE_KEY_FLAG_NON_EXPORTABLE unless there is a specific need to access the key value outside the SE.
◆ SL_SE_KEY_STORAGE_INTERNAL_IMMUTABLE
#define SL_SE_KEY_STORAGE_INTERNAL_IMMUTABLE 0x03 |
Key is one of the pre-defined keys (pre-loaded or write-once) available in the SE.
See documentation for a list of available keys.
◆ SL_SE_KEY_SLOT_VOLATILE_0
#define SL_SE_KEY_SLOT_VOLATILE_0 0x00 |
List of available internal SE key slots.
Internal volatile slot 0
◆ SL_SE_KEY_SLOT_VOLATILE_1
#define SL_SE_KEY_SLOT_VOLATILE_1 0x01 |
Internal volatile slot 1.
◆ SL_SE_KEY_SLOT_VOLATILE_2
#define SL_SE_KEY_SLOT_VOLATILE_2 0x02 |
Internal volatile slot 2.
◆ SL_SE_KEY_SLOT_VOLATILE_3
#define SL_SE_KEY_SLOT_VOLATILE_3 0x03 |
Internal volatile slot 3.
◆ SL_SE_KEY_SLOT_APPLICATION_SECURE_DEBUG_KEY
#define SL_SE_KEY_SLOT_APPLICATION_SECURE_DEBUG_KEY 0xF8 |
Internal immutable application secure debug key.
◆ SL_SE_KEY_SLOT_APPLICATION_AES_128_KEY
#define SL_SE_KEY_SLOT_APPLICATION_AES_128_KEY 0xFA |
Internal immutable application AES-128 key (bootloader key)
◆ SL_SE_KEY_SLOT_APPLICATION_SECURE_BOOT_KEY
#define SL_SE_KEY_SLOT_APPLICATION_SECURE_BOOT_KEY 0xFC |
Internal immutable application secure boot key.
◆ SL_SE_KEY_SLOT_APPLICATION_ATTESTATION_KEY
#define SL_SE_KEY_SLOT_APPLICATION_ATTESTATION_KEY 0xFE |
Internal immutable application attestation key.
◆ SL_SE_KEY_SLOT_SE_ATTESTATION_KEY
#define SL_SE_KEY_SLOT_SE_ATTESTATION_KEY 0xFF |
Internal immutable SE attestation key.
◆ SLI_SE_WRAPPED_KEY_OVERHEAD
#define SLI_SE_WRAPPED_KEY_OVERHEAD (12 + 16) |
Size overhead for wrapped keys.
Typedef Documentation
◆ sl_se_key_type_t
typedef uint32_t sl_se_key_type_t |
Supported key types.
◆ sl_se_storage_method_t
typedef uint32_t sl_se_storage_method_t |
Key storage method.
Can have one of SL_SE_KEY_STORAGE_EXTERNAL_PLAINTEXT, SL_SE_KEY_STORAGE_EXTERNAL_WRAPPED, SL_SE_KEY_STORAGE_INTERNAL_VOLATILE or SL_SE_KEY_STORAGE_INTERNAL_IMMUTABLE.
◆ sl_se_key_slot_t
typedef uint32_t sl_se_key_slot_t |
Internal SE key slot.