sl_cli_instance_parameters_t Struct Reference
The structure defining the parameters for creating a CLI instance.
#include <sl_cli_types.h>
Data Fields | |
char * | task_name |
The name. | |
sl_iostream_t * | iostream_handle |
The iostream. | |
sl_cli_command_group_t * | default_command_group |
The command_group. | |
osThreadId_t | thread_id |
Thread ID. | |
void * | thread_cb |
Thread control block. | |
void * | stack |
Pointer to the stack. | |
uint32_t | stack_size |
The stack size. | |
osPriority_t | prio |
The task priority. | |
uint32_t | start_delay_ms |
The task start delay. | |
uint32_t | loop_delay_ms |
The task loop delay. | |
The structure defining the parameters for creating a CLI instance.
Field Documentation
◆ task_name
char* sl_cli_instance_parameters_t::task_name |
The name.
◆ iostream_handle
sl_iostream_t* sl_cli_instance_parameters_t::iostream_handle |
The iostream.
◆ default_command_group
sl_cli_command_group_t* sl_cli_instance_parameters_t::default_command_group |
The command_group.
◆ thread_id
osThreadId_t sl_cli_instance_parameters_t::thread_id |
Thread ID.
◆ thread_cb
void* sl_cli_instance_parameters_t::thread_cb |
Thread control block.
Can be set to NULL for dynamic allocation.
◆ stack
void* sl_cli_instance_parameters_t::stack |
Pointer to the stack.
Can be set to NULL for dynamic allocation.
◆ stack_size
uint32_t sl_cli_instance_parameters_t::stack_size |
The stack size.
◆ prio
osPriority_t sl_cli_instance_parameters_t::prio |
The task priority.
◆ start_delay_ms
uint32_t sl_cli_instance_parameters_t::start_delay_ms |
The task start delay.
◆ loop_delay_ms
uint32_t sl_cli_instance_parameters_t::loop_delay_ms |
The task loop delay.