You are viewing documentation for version: 4.2 | Version History ... Configuration Options The API Flow Control Support ... uint16_t head; \ uint16_t tail; \ volatile uint16_t used; \
ProductMicrocontrollersResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services ... SL_SLEEPTIMER_FREQ_DIVIDER must be a power of 2 within the range 1 to 32. ... All API functions can be called from within interrupt handlers.
5.1.2 (latest) Platform# Platform (formerly known as Gecko Platform) is the foundation for Silicon Labs ... Gecko SDK will continue to be available providing long-term support for our Series 0 ...
You are viewing documentation for version: 4.2 | Version History ... RTT module uses a control block structure located in RAM memory with a specific ID so that it can be discovered when a ...
ProductMicrocontrollersResource TypeSoftware API documentation
... that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... , secure boot and secure debug implementation, is available on all series 2 devices.
Results 1-6 of 6 for gecko-platform/3.2/emlib/api/efm32zg/hardware-driver/api/group-imu-fusion