Silicon Labs
gecko-platform/3.2/emlib/api/efr32xg23/common/api/group-stdio
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
    Results 1-5 of 5 for gecko-platform/3.2/emlib/api/efr32xg23/common/api/group-stdio in 0.16 seconds
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    0 - the request failed, the contains the error message ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... WGM160P Gecko OS Plugin file_system Examples
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
    ProductWireless Resource TypeSoftware API documentation
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults counter ... system.safemode.sleep_timeout - Set the duration for which the device sleeps before rebooting.
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    ... in the examples on this page were captured with system print level ( sy p ) = all, and system command header enabled ( sy c h ) = true. ... os pins can only use the strong drive strength.
    ProductWireless Resource TypeSoftware API documentation
      Results 1-5 of 5 for gecko-platform/3.2/emlib/api/efr32xg23/common/api/group-stdio