Training ... // Gecko Platform//Version 4.4.1 //Services ... This driver works with a configurable time unit called tick. ... All API functions can be called from within interrupt handlers.
// Platform//Version 5.0.1 //Security //API Documentation //SE Manager ... is the recommended device independent crypto API and should be used whenever possible. ... Description 0 Ignore
... driver instances. The driver does not buffer or queue data. However, it queues UART transmit and receive operations. ... Simple direct/forced transmit and receive functions are also available.
ProductMicrocontrollersResource TypeSoftware API documentation
2.4 Basic Storage Basic storage is defined as the size of all the latest version of all objects, ... is documented in the EMDRV->NVM3 section of the Gecko HAL & Driver API Reference Guide.
Resource TypeUser's Guides
Results 1-6 of 6 for gecko-platform/4.0/emlib/api/efm32gg12/driver/api/structsl-simple-led-context-t