Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Device configuration and utilities (Utilities) ... Reset The device is reset. 7
// Gecko Platform//Version 4.4.1 //Services //API Documentation //Sleep Timer ... and sleeptimer.h source files for the SLEEPTIMER device driver library are in the service/sleeptimer folder.
You are viewing documentation for version: 4.2 | Version History ... Configuration Options The API Flow Control Support Example ... The UARTDRV device handle used to start the transfer.
ProductMicrocontrollersResource TypeSoftware API documentation
Results 1-6 of 6 for gecko-platform/4.0/emlib/api/efm32tg/service/api/group-device-init-hfrco