http_head http_post http_read_status ... Gecko OS writes the file to extended flash or bulk flash, depending on the location option ... c rc: CRC32 checksum of the file data, in hex format 2 .
Example Example usage. Alphabetical List of Commands ... os pins can only use the strong drive strength. ... Returns the RSSI value from the latest received packet of the current active ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
See the following for additional example demos for using the BGX13: ... boards at the start of evaluation, to ensure that the module supports all the latest features and functionality.
ProductWirelessResource TypeSoftware API documentation
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/4.0/emlib/api/efm32tg11/common/api/group-enum