Example Example usage. Alphabetical List of Commands ... os pins can only use the strong drive strength. ... stream mode, either with the str_select GPIO (see gfu ), or by issuing the the str ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS writes the file to extended flash or bulk flash, depending on the location option: -l ... Default: extended . -c <checksum> c rc: CRC32 checksum of the file data, in hex format 2 .
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS is part of a larger sophisticated application framework installed on all ... wlan.mac wlan.network.dns wlan.network.gateway wlan.network.ip wlan.network.netmask wlan.network.status
ProductWirelessResource TypeSoftware API documentation
See the following for additional example demos for using the BGX13: ... boards at the start of evaluation, to ensure that the module supports all the latest features and functionality.
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/4.0/emlib/api/efm32tg11/driver/api/struct-s-p-i-d-r-v-handle-data