Silicon Labs
gecko-platform/4.0/emlib/api/efm32xg1/common/api/group-atomic
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
    Results 1-5 of 5 for gecko-platform/4.0/emlib/api/efm32xg1/common/api/group-atomic in 0.44 seconds
    BGAPI | BGAPI headers | Bluetooth LE | v5.0 | Silicon Labs
    https://docs.silabs.com/....
    You are viewing documentation for version: 5.0 BGAPI# ... | cmd_system_stop_bluetooth | 0x01 | 0x1d | 0 | | cmd_system_get_version | 0x01 | 0x1b | 0 | | cmd_system_reset | 0x01 | 0x01 | 1 | | ...
    Micrium OS - Silicon Labs
    https://www.silabs.com/.../micrium...
    ... your multi-task application code. File System A flexible implementation of the FAT ... Micrium OS is provided entirely free of charge for deployment on Silicon Labs EFM32 and EFR32 devices!
    Resource TypeSoftware Pages
    sl_bt_evt_scanner_scan_reportScanner | Scanner | Bluetooth LE | v5.0 | Silicon Labs
    https://docs.silabs.com/.../a00...
    Support ... // Bluetooth LE//Version 5.0 //API Reference ... You are viewing documentation for version: 5.0 sl_bt_evt_scanner_scan_reportScanner# ... Value 0 indicates no periodic advertising.
    System | Bluetooth API Reference Guide | Bluetooth LE | v6.1.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-sys...
    Home ... sl_bt_evt_system_external_signal sl_bt_evt_system_awake sl_bt_evt_system_soft_timer System# System. Commands and events in this class can be used to access and query the local device.
    Resource TypeSoftware API Documentation
    Security Manager | Bluetooth Stack API Reference | Bluetooth LE | v7.1.1 | Silicon Labs
    https://docs.silabs.com/.../sl-bt...
    0: Bonding request does not need to be confirmed ... 1: Allow connections only from bonded devices Bit 5: 0: Prefer just works pairing when both options are possible based on the settings.
      Results 1-5 of 5 for gecko-platform/4.0/emlib/api/efm32xg1/common/api/group-atomic