Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
ProductWirelessResource TypeSoftware API documentation
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... Safe mode is indicated by the system.safemode.status variable.
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
BGX13-1.x Command Reference This page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... > gge 5 1 gges
ProductWirelessResource TypeSoftware API documentation
Gecko OS writes the file to extended flash or bulk flash, depending on the location ... 1 : Some options can be combined with a single dash, e.g. -de , -eu , or supplied as separate options.
Results 1-5 of 5 for gecko-platform/4.0/emlib/api/efr32xg21/service/api/structsl-cpc-endpoint-debug-counters-t