... control on devices that don't have UART CTS/RTS hardware support, the driver includes the GPIOINT driver to emulate a hardware implementation of UART CTS/RTS flow control on these devices.
ProductMicrocontrollersResource TypeSoftware API documentation
Home ... 5.1.2 (latest) Platform# Platform (formerly known as Gecko Platform) is the ... Table of Contents Platform Platform Components Version HistorySupportAbout UsCommunityContact UsPrivacy ...
// Gecko Platform//Version 4.4.1 //Services ... The hardware timer peripheral must be properly clocked from the application. ... All API functions can be called from within interrupt handlers.
Results 1-6 of 6 for gecko-platform/4.0/emlib/api/efr32xg22/service/api/structsl-se-command-context-t