psa_drv_se_t Struct Reference
A structure containing pointers to all the entry points of a secure element driver.
#include <crypto_se_driver.h>
Public Member Functions | |
uint32_t | MBEDTLS_PRIVATE (hal_version) |
The version of the driver HAL that this driver implements. | |
size_t | MBEDTLS_PRIVATE (persistent_data_size) |
The size of the driver's persistent data in bytes. | |
psa_drv_se_init_t | MBEDTLS_PRIVATE (p_init) |
The driver initialization function. | |
const psa_drv_se_key_management_t * | MBEDTLS_PRIVATE (key_management) |
const psa_drv_se_mac_t * | MBEDTLS_PRIVATE (mac) |
const psa_drv_se_cipher_t * | MBEDTLS_PRIVATE (cipher) |
const psa_drv_se_aead_t * | MBEDTLS_PRIVATE (aead) |
const psa_drv_se_asymmetric_t * | MBEDTLS_PRIVATE (asymmetric) |
const psa_drv_se_key_derivation_t * | MBEDTLS_PRIVATE (derivation) |
A structure containing pointers to all the entry points of a secure element driver.
Future versions of this specification may add extra substructures at the end of this structure.
Member Function Documentation
◆ MBEDTLS_PRIVATE() [1/3]
uint32_t psa_drv_se_t::MBEDTLS_PRIVATE | ( | hal_version |
| ) |
The version of the driver HAL that this driver implements.
This is a protection against loading driver binaries built against a different version of this specification. Use PSA_DRV_SE_HAL_VERSION.
◆ MBEDTLS_PRIVATE() [2/3]
size_t psa_drv_se_t::MBEDTLS_PRIVATE | ( | persistent_data_size |
| ) |
The size of the driver's persistent data in bytes.
This can be 0 if the driver does not need persistent data.
See the documentation of psa_drv_se_context_t::persistent_data for more information about why and how a driver can use persistent data.
◆ MBEDTLS_PRIVATE() [3/3]
psa_drv_se_init_t psa_drv_se_t::MBEDTLS_PRIVATE | ( | p_init |
| ) |
The driver initialization function.
This function is called once during the initialization of the PSA Cryptography subsystem, before any other function of the driver is called. If this function returns a failure status, the driver will be unusable, at least until the next system reset.
If this field is NULL
, it is equivalent to a function that does nothing and returns PSA_SUCCESS.