Silicon Labs
gecko-platform/4.1/emlib/api/efm32lg/service/api/structsl-power-manager-em-transition-event-handle-t
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
    Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32lg/service/api/structsl-power-manager-em-transition-event-handle-t in 0.19 seconds
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    0 - the request failed, the contains the error message ... If omitted, file version defaults to 1.0.0 . -t <type> t ype: specify file type as integer or hex string 2 .
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... 0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults ...
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Command data types. ... Issue Gecko OS command, store string result in buffer. ... More. gos_result_t gos_cmd_issue_with_config ( gos_cmd_operation_config_t *config, const char *fmt,.)
    ProductWireless Resource TypeSoftware API documentation
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    ... response headers. See Serial Interface, Response Format . Documentation for each ... os pins can only use the strong drive strength. ... > gfu 0 con_status_led Success > gdi 0 ohi od Success
    ProductWireless Resource TypeSoftware API documentation
      Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32lg/service/api/structsl-power-manager-em-transition-event-handle-t