Silicon Labs
gecko-platform/4.1/emlib/api/efm32tg11/service/api/group-version
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
    Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32tg11/service/api/group-version in 0.28 seconds
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... 0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults ... ls
    ProductWireless Resource TypeSoftware API documentation
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    BGX13-1.x Command Reference This page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... > gge 5 1 gges
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    1 - an update is available, the contains the new bundle version string ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... ipd 1 Input, high-impedance
      Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32tg11/service/api/group-version