You are viewing documentation for version: 4.2 | Version History ... Functions sl_status_t sl_iostream_rtt_init (void) ... Returns ... sl_iostream_instance_info_t sl_iostream_instance_rtt_info
ProductMicrocontrollersResource TypeSoftware API documentation
... example the device will erase OTP and become inoperable if 4 glitch signals is seen in a 1 minute time period. ... This command is only available once! sl_se_init_otp(&otp_settings_init);
Home ... // Gecko Platform//Version 4.4.1 //Services //API Documentation //Sleep Timer ... All API functions can be called from within interrupt handlers. ... Expected value: 1-31. uint8_t N/A