// Gecko Platform//Version 4.4.1 //Services //API Documentation //Sleep Timer ... and sleeptimer.h source files for the SLEEPTIMER device driver library are in the service/sleeptimer folder.
Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Device configuration and utilities (Utilities) ... Reset The device is reset. 7
You are viewing documentation for version: 4.2 | Version History ... Configuration Options The API Flow Control Support Example ... The UARTDRV device handle used to start the transfer.
ProductMicrocontrollersResource TypeSoftware API documentation