Silicon Labs
gecko-platform/4.1/emlib/api/efm32xg12/service/api/structsl-power-manager-em-transition-event-info-t
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
Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32xg12/service/api/structsl-power-manager-em-transition-event-info-t in 0.16 seconds
Gecko OS Commands Silicon Labs
https://docs.silabs.com/.../comma...
2 - no update available (i.e. the device's current firmware is up-to-date) <message> - bundle version or ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ...
Gecko OS 4.2 Command API Silicon Labs
https://docs.silabs.com/.../...
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Commands - v4.1 - Gecko OS API Documentation Silicon Labs
https://docs.silabs.com/.../group-api-core-comm...
Commands Core Functions for issuing Gecko OS commands. More. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API . ... fmt Formatted Gecko OS serial command Returns
ProductWireless Resource TypeSoftware API documentation
Bluetooth SDK Release Notes
https://www.silabs.com/.../bt-software-release-notes-7.3.0.0....
OS timer frequency configuration parameters that can be set to modify the timer ... API references and other information about this and earlier releases is available on https://docs.silabs.com ...
Resource TypeRelease Notes
Getting Started with Bluetooth Xpress - v1.0 - Gecko OS API Documentation Silicon Labs
https://docs.silabs.com/.../getting-star...
... with BGX modules using the Xpress framework, which provides a simple API for BGX interaction. ... both the streaming interface and the Xpress command API through remote command execution.
ProductWireless Resource TypeSoftware API documentation
    Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32xg12/service/api/structsl-power-manager-em-transition-event-info-t