File is p re-encrypted using the system.security_key ( user key). ... 2 : hex format: upper or lower case, with leading 0x , e.g. 0xFE , 0xe1c8 ... WGM160P Gecko OS Plugin file_system Examples
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
ProductWirelessResource TypeSoftware API documentation
... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... > gfu 2 str_select Success > gdi 2 ipuw db3 Success
ProductWirelessResource TypeSoftware API documentation
... with BGX modules using the Xpress framework, which provides a simple API for BGX interaction. ... both the streaming interface and the Xpress command API through remote command execution.
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32zg/service/api/group-se-mac